Part Number: TLC5957 Hi Team,
What is the Viref to be used for calculating Riref with 10mA (constant current) and BC=4H(gain =100)?
In the datasheet the reference voltage is specified for a test condition.(1mA)
Can the same be used or can you provide…
Part Number: TLC5957 Hi,
Does LAT pin on this IC TLC5957 can be used as a chip select pin ? If not, please clarify which pin can be used as SPI chip select pin ?
Regards,
Srivatsan.R
Part Number: TLC5957 Other Parts Discussed in Thread: TLC59581 , TLC6946 Hi,
1. TLC5957RTQR Supports daisy chain mode? As I want to interface 2 TLC5957RTQR. But in my MCU only one SPI available.
2. Do you have any SPI timing analysis data for to know…
Part Number: TLC5957 I'm building a 16x16 LED matrix. According to the spec. description and the sample code, send First Line data, then input 65535 GCLK and the 2nd line data, repeat it 15 times. Then repeat the input of data and GCLK in a loop.
…
Part Number: TLC5957 I'm using the TLC5957 chip, with 40 of them daisy-chained together. I've managed to derive how to push LED brightnesses to all the chips, but I'm still puzzled regarding writing and reading FC registers. When I send a "read FC" command…
Part Number: TLC5957 Tool/software: Code Composer Studio The app note #SLVUAF0 from May 2016 says "The output of the LOD detect circuit is loaded into the 48-bit register called SID holder", but that is the extent of the mention of the "SID holder" register…
Part Number: TLC5957 Other Parts Discussed in Thread: TLC59581 , TLC59582 , TLC59213 Hi,
I have to make a Signage LED display drivers with a matrice led of 7x56 RGB LEDs .
I found the AN SLVUAF0. Is the TLC5957 best component for my applcation ?
Is there…
Part Number: TLC5957 Any input is much appreciated!
1. Is there example code for any of the following that will be applicable when using a daisy chain configuration besides what is described in the app note SLVUAF0?
a. - example setting the FC regi…