Part Number: TLC6C5712-Q1 Hi team,
When LED supply drops and WLS fault is detected, is LED diagnostic still functioning in parallel? E.g., will LED open fault get reported since LED supply is low which may result in LED open fault?
After software POR…
Part Number: TLC6C5712-Q1 Hi team,
I would like to minimize standby power of this device.
I don't think there is any low power mode of operation in this device, correct?
The lowest power consumption can be achieved by disabling all the channel by…
Part Number: TLC6C5712-Q1 Hi experts,
1. TLC6c5712 datasheet showing input signal and output signal diagrams on Figure 1 and Figure 2. Figure 1 is for input and Figure 2 is for output, but the two pictures are the same. Is there any typo here?
2. What…
Part Number: TLC6C5712-Q1 Hi team,
I have 2 questions of TLC6C5712Q1:
1) Suppose I have two groups of LEDs, each controlled by two LED Drivers The requirement is that these two sets of LEDs need to be on/off at the same time, will there be a delay in…
Part Number: TLC6C5712-Q1 Hi team,
For FMEA analysis, I would like to know if I can detect OPEN or SHORT failure of OUTx transistors in the device?
And if yes, will it be reported to /ERR pin?
For OUTx transistor SHORT failure,
Is that detected as LED…
Part Number: TLC6C5712-Q1 Other Parts Discussed in Thread: TLC6C5912 Hi team,
I know this device is constant current regulator, but is it possible to use it as TLC6C5912 by using external resistor to set the LED current?
If I select the external resistor…
Part Number: TLC6C5712-Q1 Hi team,
Is there an apps note describing the detail of Open-Load, Adjacent pin short, PWM input frequency supervision diagnostic feature?
I would like to know.
1. LED Open Load detection
- mechanism of how to detect the open…
Part Number: TLC6C5712-Q1 Hello, Team,
1. Would like to double check: Is outputting 50mA from all 12 channels (12ch * 50mA = total 600mA) simultaneously using TC6C7512-Q1 ok?
2. For the thermal, it will be taken care so that it operates below absmax given…
Part Number: TLC6C5712-Q1 Hi, Team,
The customer has two questions:
Is it ok to tie OUT0, OUT2, OUT6, OUT8 output pins to supply current to a single LED?
When tying multiple outputs to supply current to a single LED, does it have to be either even or…
Part Number: TLC6C5912-Q1 Other Parts Discussed in Thread: TLC6C5816-Q1 , TLC6C5712-Q1 Hi team,
In datasheet, there are description about clear register. Please tell me recommended time which do input logic low from power on.
And also want to know when…