Part Number: TLC5951 Other Parts Discussed in Thread: TLC6C5724-Q1 , Dear team,
My customer was using TLC6C5724-Q1 but due to supply issue, they need to use some TLC5951 in the same socket. Those two devices can be P2P replaced considering the DCSIN, DCSOUT…
Part Number: TLC6C5716-Q1 Other Parts Discussed in Thread: TLC6C5724-Q1
Tool/software:
Hi Team,
Do we have FMEDA and safety manual for TLC6C5716-Q1 and TLC6C5724-Q1 ? Please help send email to me.
Thank you!
Marc
Part Number: TLC6C5724-Q1 Hello,
We are using TLC6C5724-Q1 to drive dashboard tell tale leds and in actual configuration we are always seing ERR pin "Low" even if all the pins are connected.
Checked with the EVM module and the same cluster…
Part Number: TLC6C5724-Q1 We are currently using TLC6C5724-Q1 to drive the 6 LED drivers in daisychain.
1)We are supposed to analyse the propagation delay.
Assuming the peripheral clock for SPI from uc is(SCLK) --->500Khz
i bit to be shifted …
Part Number: TLC6C5724-Q1 Hi Team,
1.My doubt is we can only configure the device either with Grayscale configuration or FC-BC-DC am I right ?
2.what is the purpose of blank signal when we are using FC-BC-DC configuration?
Figure 2 in date sheet is little…
Part Number: TLC6C5724-Q1 Hello Team,
As the title describes, I could not find any information in the datasheet on how long it takes the ERROR pin to assert once a Fault is detected for this device. Basically, do we have data on the propagation delay…
Part Number: TLC6C5724-Q1 Hi team,
According to previous E2E thread below, customer expects V(out,min) is less than 0.7V.
But in actual measurement result in attached file shows V(out,min) = 1.6V with "Vcc=5V, Iout=50mA, V_LEDsupply=4.2V" condition..…
Part Number: TLC6C5724-Q1 Hello,
i am trying to find our the difference betyween the references PTLC6C5724QDAPRQ1 and TLC6C5724QDAPRQ1, but i cannot see it what is the meaning of the prefix P, can anyone help me?
thnaks and regards.
Part Number: TLC6C5724-Q1 Hi
I would like to ask how to calculate the TLC6C5724Q1 power dissipation, what parameters should we need to calculate? Thank you.