Part Number: TLE4275-Q1 Hi E2E,
When our customer using the TLE4275QKVURQ1 to replace ON-NCV4275.
There is a difference between them:
Application scenario: 12V to 5V, load 10-20mA, Cout=22uF.
Abnormal phenomenon: the output voltage has periodic…
Part Number: TLE4275-Q1 Dear team,
My customer use our TLE4275-Q1, and they found some strange phenomenon. For some chips, the output has 234mV ripple as the second picture. When they remove TLE4275's all load, the ripple disappears.
TLE4275-Q1 has…
Part Number: TLE4275-Q1 Dear TI Team,
We are using TLE4275-Q1 and the query is regarding Reset out (Pin 2) of LDO.
As per the datasheet, reset delay can be vary depending on Cap value. which is around 15.4mSec by using 47nF cap.
Also, as per the formula…
Part Number: TLE4275-Q1 Other Parts Discussed in Thread: TPS7B68-Q1 , TPS7A66-Q1 , TPS7B81-Q1 , TPS7B81 Hi Team,
My customer use TLE4275 to change 12V to 5V. The load current is blew 100mA...
And TLE4275 is screaming and have a loudly noise, which can be heard…
Part Number: TLE4275-Q1 Hello team, customer is looking for stability data with following input:
Input cap =
1)1*10uF=10uF 25V 1206
Part no: GCJ31CR71C106KA15L
2)1*100nF=100nF 50V
Part no:GCJ21BR71H104KA01L
Output Cap=10uF*3=30uF 0805
Part no:C2012X…
Part Number: TLE4275-Q1 Hello all,
I am doing stability analysis for the TLE4275 -Q1 IC by NON INVASIVE METHOD,
MY PHASE MARGIN MEASURED IS 8 DEGREE It is too low to pass the requirement
I have tried adding 1 Ohm Resistor in Series with the alll 3*10uF…
Part Number: TLE4275-Q1 Hi Team,
May I ask:
Pin8 and Pin13 need to connect to GND?
Pin17,Pin18 and Pin 19 need to connect together?
The thermal pad need to connect to GND?
Thanks!
Part Number: TLE4275-Q1 Hi Team,
My customer found TLE4275QKTTRQ1 gets oscillating on their prototype board.
Attached is the test circuitry they made for evaluation.
Q.1) Pleas check attached material. (Highest priority)
It looks nothing wrong in setup…
Part Number: TLE4275-Q1 Hi Team,
When user doesn't use Delay and Reset function, could how RESET and DELAY port should be terminated?
Is it OK with below?
- RESET : open
- DELAY : Short to GND
Best regards,
Part Number: TLE4275-Q1 VCC=5V BATTERY=0V
We have used TLE4275-Q1 as load when down the F/W. we found the VCC (from USB) is instability ,so that the down failure. Could you help check What caused the issue ,Leakage currentor capacitive load,and so on
PS…