Part Number: TLK2711-SP Other Parts Discussed in Thread: TLK2711EVM-CVAL Hello,
I have a question regarding the datasheet of the TLK2711-SP : www.ti.com/.../tlk2711-sp.pdf
In Section 5.6 – Transmitter/Receiver Electrical Characteristics. The parameter…
Part Number: TLK2711-SP We are planning to develop a board based on the following architecture and intend to use a single TLK2711-SP device.
Our intended configuration is:
RXP/RXN (receiver side): connected to a sensor payload
TXP/TXN (transmitter…
Part Number: TLK2711-SP Hi Experts,
Would you kindly check the schematic below and confirm if the pullup, pulldown and caps are enough?
Thanks and regards,
Marvin
Part Number: TLK2711-SP Regarding TLK2711-SP, we have the following questions.
1. Packing configuration
Could you please advise on the packing configuration?
If available, we would appreciate it if you could share the tray drawing and information…
Part Number: TLK2711-SP Tool/software: Hello,
In our application, two TLK2711s share the same power supply line. Both operate in Tx only mode, but only one at a time (one is enabled and the other is disabled). If an over-voltage on the power rail exceeds…
Part Number: TLK2711-SP Hi,
I wanted to finalize VDDA supply filtering ferrite bead specifications, regarding this I have few queries-
What should be its impedance ( at 100 MHz)? EVM is having 600 Ohm whereas in Datasheet Figure 7-1 , 5 Ohm Ferrite…
Part Number: TLK2711-SP Other Parts Discussed in Thread: LMK00804B , Tool/software: Dear,
I'll use TLK-2711SP with kintex7 fpga like below figure.
Unfortunately, FPGA clocks have poor jitter characteristics. So, I think I will try to design…
Part Number: TLK2711-SP Tool/software: Hello,
Im using the TLK2711-SP in transmit only mode and I am seeing voltage on the VDD/VDDA pin even though it is not powered.
Here is the setup:
The TLK2711-SP is setup to be in only transmit mode, the…
Part Number: TLK2711-SP Dear sir/ madam,
kindly provide SEU LETth for below mentioned part number since this data is not available in the technical data sheet.
5962-0522101VXC/TLK2711-SP
Part Number: TLK2711-SP Tool/software: For FMEA analysis, we need to know if there is adequate protection of the TLK2711-SP's driver in the case that the far end receiver has one pin shorted to GND (or Vcc). We could not find any such info within the…