Part Number: TLV1851-Q1 Tool/software: I just want to confirm that the input leakage with 0V supply will be ~55nA when IN+/- are at a positive voltage. Essentially, same behavior as seen in the 1.8V supply plot (Figure 6-9) in the datasheet, but with…
Part Number: TLV1851-Q1 Other Parts Discussed in Thread: TLV1851 , ATL431 , TL331B Hello, I have TLV1851 with 3v3 supply, IN- @ 2.5V using for PWM logic level translation from 5Vmax, 7Vmax, 10Vmax pwm signals. Output is high impedance, and actually the…
Hi Eric,
I apologize for the confusion. This device is old, and the datasheet hasn't been revised in a while. Your circuit would work as the TLV3701-Q1 has over-the-rail operation, which means the inputs can go over the rail (VCC < VIN < VCC + 5V…
Part Number: TLV1811-Q1 Other Parts Discussed in Thread: TLV3701 , TLV1811 , TLV1851 I was using the TLV370X series parts these parts are no longer recommended for new designs. Looking at parts, I feel the TLV1811 would be a more appropriate replacement…
Part Number: TXH0137D-Q1 Other Parts Discussed in Thread: TLV1872 , TLV1851 , TLV9030 , TL431 , ATL431 Tool/software: Hi Sirs, Does TI provide a level shifter to compatible with wide input range from 1.2V to 12V, fixed 3.3V push-pull output for logic…