Part Number: TLV2217 Tool/software: For a new design we need a dual supply for an instrumentation opamp where we need a differential analog output between -10V and +10V.
So we need a double supply for the opamp. The operaring voltage for this instrumentation…
Part Number: TLV2217
Hello,
I have a client that wants to power a device with battery voltages ranging from 3 V to 12 V. The required device voltage is 3-3.3 V, so we used the TLV2217-33. I designed the power circuit to have a battery plug-in that…
Patrick,
Based on using the 30 Ohm in series, if the output load is constant, then the input voltage directly to the TLV2217 should be about 11.1V, which should not cause any issues.
Based on using the 70 Ohm in series, if the output load is constant…
Part Number: MC3303 Other Parts Discussed in Thread: TL760M33-Q1 , TLV2217
Hello,
SiliconExpert Technologies has been contracted by our customer to work with their suppliers to collect component information. We would appreciate your support to provide…
Hi Wesley,
The UA78M has a recommended operating temperature range of -40 to 125C. I suspect that below -40C the bandgap reference circuit is having an issue with starting up. The TLV2217 is a newer device (1992 vs the UA78 being released in 1976…
Hello Ming,
Thanks for the quick response.
Could you help me out with one more thing please?
If the Vsys operates in the ranges of 7.4V Vbat ~ 12V adapter, I need a LDO regulator to supply TLV320AIC3104 codec and BT IC with 1.8V, 3.3V, and 5.0V…
Hi Nick,
Thanks for your response.
We have tested TPS7B8733QKVURQ1, TPS7B8833QKVURQ1, TPS7B8633QKVURQ1 & TL760M33QKTTRQ1 LDO part at 24VDC.
TLV2217-33KVURG3 we tested at 12 VDC input voltage.
Working temperature is temperature measured at…