Part Number: TLV2472 Hello, We are checking whether the tube length of the TLV2472IDGN is acceptable for our EMS supplier's tool (as an alternate to the TLV2472IDGNR).
Can you please help advise what the tube length of TLV2472IDGN is?
Part Number: TLV2472A Other Parts Discussed in Thread: TLV2472 , Hi,
As far as I can see the DS, TLV2472 and TLV2472A seem to differ only in offset MAX.
Customers are considering changing from TLV2472A to TLV2472 due to delivery issues.
I think…
Hi Ron,
Thank you for your explanation, i just calculate my test result by your equation and the gain is quite stable.
my another question, i used same resistor value, same brand for 2 TLV2472, but the result is different.
so i have to do trial and…
Other Parts Discussed in Thread: TLV2472 Hi,
I'm working with the precision amplifier TLV2472 and I've been surprised to see that it's not working if the input voltage is less than 0.5V.
I'd like to know if this is normal and why. Also, if the…
Hi Shambhulingayya,
When I review the various DSO images you captured I still come to the conclusion that the waveform is that of an unintended oscillation condition, and not that of the intended, controlled frequency output. The original TI Analog…
Hi Jeff,
We were able to find the data for these devices:
• TLV2472/4 pass 2kV HBM, 1kV CDM.
• TLV274-Q1 pass 2kV HBM, 1kV CDM.
• TLE2071A pass 1kV HBM, 1kV CDM.
As far as adding to the datasheets, we will take this feedback and add it to our…
Hi Sravya,
Attached is the C2000 PCB design guide PDF and very good to review even if you are an avid PCB designer.
Regards,
TI-F2800x Hardware Design Guidelines for TMS320F28xx and.pdf
Hi,
an additional document, which might be very useful, is an application report on single supply OPAs Single-Supply_Op_Amp_Design_Techniques_sloa030a_2001_03.pdf
Best regards
Peter
The OPA145 also looks like a good choice, this file has not been recently updated so the OPA196 is not in yet, and the pricing is out of date.
OPA111A options.xlsx