Thanks for response.
The incoming signal is square wave.
supply voltage is 3.3V.
Are you suspecting this because of speed limit in TLV3202 device.
Reference voltage is fixed one verified no distortion.
Part Number: TLV3202 Hello,
I would like you to confirm about Vcc condition at figure 17(Propagation Delay Falling Edge) and figure 18(Propagation Delay Rising Edge).
* According to figure 17 and 18, output voltage is approx 5.2V (+/- 2.6V).
On the other…
Hi Shreeneet,
TLV7012 (dual push pull) should be ok for this application. I only recommended TLV903x and TLV3202 as they have better speed capabilities and accuracy which would be helpful in terms of phase lag and duty cycle of the waveforms. TLV9034…
Part Number: TLV3202 Other Parts Discussed in Thread: TLV3502 Support Path: /Product/Help with Device Selection/Amplifier/filter solution/ Good morning,
I'm designing an application based on a FPGA. The chip needs fast transition at its inputs pi…
Other Parts Discussed in Thread: TLV3202 , LM2904 , LM2903 , TLV3201 , LMV7272 Hi Team:
My customer use below circuit.
U145 if they use TLV3202, the DAO1(Comparator input pin) will be like below:
If they replace the TLV3202 with LM2904, the output will be…
Part Number: TLV9032 Other Parts Discussed in Thread: TLV9022 , , TLV3202 Hello,
The Datasheet (Table 6.9) describes the max toggle Frequency (F_TOGGLE) for the TLV9022 (Open Drain version) being ~3MHz (typ) with V_S= 5V. What might the worst case (typ…
Hi Lennon,
Unless a particular specification has a maximum, or minimum, specified in the Electrical Characteristics table, then we cannot state one. Doing so would infer that TI is assuring a levels of performance that reside outside the data sheet. A …
Hello Narendra,
A very fast 5 V CMOS comparator that is available in the 8-pin SOIC (D) package is the TLV3501. It has a typical propagation delay time of 4.5 ns, and maximum of 6.4 ns (TA = 25 C).
https://www.ti.com/lit/ds/symlink/tlv3502.pdf
A bit of…