Part Number: TLV320ADC3140 I am designing a multichannel audio acquisition system using the TLV320ADC3140 configured in TDM Slave Mode. BCLK and FSYNC are provided by an external digital master processor.
While performing high-frequency testing, specifically…
Part Number: TLV320ADC3140 Other Parts Discussed in Thread: TAS5805 Hi,
Please kindly check below issue:
TLV320ADC3140 6DMIC
TLV320ADC3140 2Echo_reference
TAS5805 output connected to 2Echo_deference
The software was tested for simultaneous…
Part Number: TLV320ADC3140 Hi team,
My customer are using pseudo-differential traces for the microphone connection to the TLV320ADC3140. If we configure the TLV320ADC3140 input as single-ended, will this cause the pseudo-differential noise immunity…
Part Number: TLV320ADC3140 Hello:
The TI reference manual can be found at www.ti.com/.../sbaa383 . In Section 3.2, ASI Configuration for Daisy Chain TDM, it is mentioned that two registers, ASI_CFG2 0x9 and GPIO_CFG0 0x21, need to be configured. However…
Part Number: TLV320ADC3140 Hello:
The client's robot project utilizes TI's TLV320ADC3140 for data acquisition. Could you please assist in checking the circuit design for this component? Thank you! 1. Could you please check if there are any issues with…
Part Number: TLV320ADC3140 Hi
1. What could be the problem if the TLV320ADC3140 reads a value of 0xFF from the SW_RESET Register (page = 0x00, address = 0x01)?
2. Why does the reference board read an address of 0x54 instead of the 4C~4F range stated…
Part Number: TLV320ADC3140 Link introduction : SOC and U1 are located on the mainboard, with U1 receiving the speaker signal. After passing through U1, the 12S signal is transmitted through a buffer (delay 1-11ns) and then through a 700mm wire (delay…
Part Number: TLV320ADC3140 Hi ,
From datasheet,I only see figure 3. TDM (With BCLK_POL = 1), I 2S, and LJ Interface Timing Diagram .The current software configuration is bclc_pol=0, fsync_pol=0.Is there a Timing Diagram for this configuration?
Part Number: TLV320ADC3140 Tool/software: Hello,
I'm experiencing issues with recording audio using the TLV320ADC3140 codec on the TI AM62 processor. Despite configuring the device tree and adjusting gain settings, I'm unable to capture any audio. The…