Hi Jeff-san,
Sorry for the late reply. I explained this to the customer. The customer was convinced. Thank you for your support. Best Regards, Ishiwata
Part Number: TLV320ADC6120 Other Parts Discussed in Thread: ADC6120EVM-PDK , PUREPATHCONSOLE Dear Sir/Madam,
We’ve purchased the ADC6120EVM-PDK from Digikey (20230713015):
The board has arrived.
Please help to speed up the approval process for…
Part Number: TLV320ADC6120 Hi team,
TLV320ADC6120 has VAD function. The datasheet states that the TLV320ADC6120 continuously monitors one of the input channels for voice detection. So when using VAD function, should we always configure one channel as…
Part Number: TLV320ADC6120
Hi I am using PurePath. Version 3.2.1. The datasheet says that the channel gain can be set in 1d = 0.5dB increments, but on PurePath, 1d = 1dB. If you set the gain in PurePath, you will get only half of the expected gain. Also…
Hi Ore,
Thank you very much for this valuable information. It has resolved my issue.
Channel gain is used in receiver DSP algorithms of our modem. It helps to estimate a signal quality because the higher is gain the lower is the signal quality in common…
Sanjay Dixit said: 1. Is the selection single ended DC Coupled Mode.
Yes.
Sanjay Dixit said: Do you mean we have a signal with a positive peak of 1.4v and a Negative Peak of -1.4v?
Yes, obviously the signal appears distorted, but Vref/2 seems to be the…
Part Number: TLV320ADC6120 Hi teams,
Is it possible to leverage both the function of DRE and the function of AGC in TLV320ADC6120?
Best regards,
Shunsuke Yamamoto
Part Number: TLV320ADC6120
Good afternoon. Im trying to configure this CODEC as the bus master to output I2S audio data at 48KHz. I have 19.2MHz input into GPI2 and I have the following register configuration (sent to the device in this order):
uint8_t…
Part Number: TLV320ADC6120 Hello, I'm developing an acquistion board using the TLV320ADC6120
I have an input signal with amplitude +/- 2Vpp cetered at 0V.
I used MICBIAS/2 output to shift the signal to the range 0-2.75V, is it correct to use this…
Part Number: TLV320ADC6120
Hi team,
Is it possible for TLV320ADC6120 to use a fixed PGA gain value?
Because my customer determines the PGA gain value by themselves regarding the input signal above fixed threshold level.
Best regards,
Shunsuke Yamamo…