Part Number: TLV320AIC12K Hi
Customer has following question.
In datasheet pg 26 has following description
"During the first 64 MCLKs, FS is configured as an output and FSD as an input. During the next 64 MCLKs, FS is configured as an input and FSD…
Part Number: TLV320AIC12K Dear all,
I'm using TLV320AIC12K for the audio service. CRs is configed as follows:
R2:0x60
R4:0x94
R4:0x41
R5:0x3a
R5:0x6a
R3:0x08
R6:0x02
R1:0x61
TLV320AIC12K codec is configed as a master and MCLK is 20.48M. DOUT pin outputs…
Hi Steve Wilson ,
Sorry for delay in response.
Repeating my problem statement again: Need to replace codec TLV320AIC12K with mobile category codec .
We are using Audio Codec TLV320AIC12K in one of our product . In existing design, TLV320AIC12K 's connected…
Part Number: DIX4192 Hi, Can I interface 8 number of tlv320 aic12k mono codec in cascade mode directly with DIX4192? Requirement : transmit and receive 8 channels of voice over optical link
Hi,
I am a student in china. Firstly, I am sorry for my poor English. I am facing the same question as yours. I use MSP430 as master and use AIC12K as slave, but as you described before, I can just read register data, but can not write into. I can only…
What is the absolute maximum analog input voltage? Are there any clamps to protect the input? I have a customer that needs to know this so he can make sure that he is able to protect the inputs during an over-voltage event.
Thanks for your help with this…
Other Parts Discussed in Thread: TLV320AIC12K Hi Team, I found VIH as the following but couldn't find VIL for digital input pin. ----------------------------------------------- [TLV320AIC12K datasheet page.7] (1) For VIH (Input high level), when IOVDD …
Other Parts Discussed in Thread: TLV320AIC12K Hi,
I'm working on an old design with the TLV320AIC12K CODEC, and am trying to figure out how the thermal pad on the QFN (RHB) package should be connected because on our old design the connection appears…
Other Parts Discussed in Thread: TLV320AIC13 , TLV320AIC12K Hello.
Difference of TLV320AIC12K and TLV320AIC13 in datasheet that TLV320AIC12K has 8Ohm speaker driver.
Price of TLV320AIC12K is $1.6, but price of TLV320AIC13 is $6.8 and NRND.
I want to know exact…
Other Parts Discussed in Thread: TLV320AIC12K Hi,
I am planning to use TLV320AIC12k in an audio application. I wanted to know if it was a wise decision to use it in my design, as it is a pretty old chip. While I also compared it with newer versions of the…