Part Number: TLV320AIC3110 Hi,
I'm new to using the TLV320AIC3110 and have been trying to get basic headphone operation working using the Example Register Setup to Play Digital Data Through DAC and Headphone/Speaker Outputs documented in section 7.3…
Part Number: TLV320AIC3110 We are debugging Audio IC TLV320AIC3110 sent by FPGA signal to TI. The sound output will be truncated if the signal is higher than about 2.3v, resulting in noise in the sound output. If the volume input is small, there will…
Part Number: TLV320AIC3110
Hi,
If PLL P/R/J register value is changed while device working, does PLL frequency vary immediately?
(I'm recognizing that its control is not recommended.)
Best Regards,
Kuramochi
Part Number: TLV320AIC3110 Dear Sir,
We checked AIC3110 DRC have some questions need your help,
Register:
Page0 REG68 0x44( DRC Control 1)
Enable
Page1 REG38 0x26 (Left Analog Vol to SPL)
91
Page1 REG42 0x2A (SPL Driver)
0C
Page0 REG65 0x4…
Part Number: TLV320AIC3110 Hi,
my customer is using this device as below:
They use only SPRM and SPRP for both speaker and earphone.
When earphone is not connected, pin3/6 and pin4/5 are connected to one speaker.
When earphone connected, speaker is…
Part Number: TLV320AIC3110 Dear Steve,
Continuous last questions for beep and wave generate for sine wave play.
1. Do we need setting different speaker output gain tables for beep and wav. playback?
- As know, the page1 0x26, 0x2a, and page0 0x41, 0x47…
Part Number: TLV320AIC3110 Hello,
We are using TLV320AIC3110 to drive speakers and a electret condenser mic from a processor and I wanted to get my schematic verified. Could you please take a look and provide any issues/improvements.
The questions I have…
Ian,
Download Purepath Studio, This will allow you to program the MiniDSP. you will need to put together some kind of process flow. I assume they will still want to mix the Audio from the ADC, the Audio from the I2S and the Tone?
once they create a process…
Part Number: TLV320AIC3110 The datasheet and other posts imply that the AIC3110 detects headset insertion by looking at a 4th contact on the headphone jack socket. Is this the case or is there some cunning means to detect with just the L-R and GND wires…
Part Number: TLV320AIC3110 Sir,
We setting pag1/Register 42(0x2a) set to 0x00, It should means mute(no output sound) due to D2 is "0" but we still can hear sound from speaker.
Do you have idea what we can check?
Thanks, Ian.