Part Number: TLV320AIC3120 Tool/software: Hi Team,
We are looking for I2S based audio design, part we are considered to use is TLV320AIC3120IRHBT. Since TLV320AIC3120IRHBT is used as Slave mode in our application, can you please help in finding the appropriate…
You can look at this high-level summary for some of the devices. AIC3106 DMIC is on GPIO1 and GPIO2 for example which you can use but check against your requirement from the list.
7317.AIC products.pdf
Part Number: TLV320AIC3120 Hi,
We are trying to do headset jack detection functionality in TLV320AIC3120. We are following below steps:
Configured 0x88 in Page 0 / Register 67 (0x43) - To enable headset jack detection
Configured 0x81 in Page 0 / Register…
Part Number: TLV320AIC3120
Hi, I have tried different sample codes from the forum and the internet but have not been able to get any output from the speaker. Following are the commands i have prepared and correlated with the datasheet, all I2C commands…
Part Number: TLV320AIC3120
Hi,
We are evaluating the TLV320AIC3120 codec using the TLV320AIC3120EVM-U. The EVM is detected in the Device manager as well as Sound device list as USB-Mini EVM in Windows 11.
But when we open the CodecControl application…
Part Number: TLV320AIC3120 Hi,
In our board, we are using TLV320AIC3120 Codec chip. In that we have enabled headset jack detection functionality by configuring page 0 / register 67 register and also configured Page 0 / Register 48 for INT1 generation.
Then…
Part Number: TLV320AIC3120 Dear team, I am using TLV320AIC3120 AUDIO CODEC. I'd like to have some information about these below.
1) When using I2S related pins (VDD18) and SDA/SCL (PU VCC_1.8V), does IOVDD also need to supply 1.8V power?
2) Is simultaneous…
Part Number: TLV320AIC3120 Hi
Can I use this codec for signals up to 50kHz (special application) considering the audio signals are limited to 20kHz?
thank you
Part Number: TLV320AIC3120 I'm starting to think I'm missing something fundamental in the TLV320AIC3120 functionality.. I've got a custom PCB built. Its only purpose in life (right now) is to take the input from the microphone and amplify it…
Part Number: TLV320AIC3120 Hello Expert,
I have two questions as follows and if you could write your opinion on each item.
1. I plan to use AUDIO CODEC only as slave.
Can I just connect SDIN and open SDOUT?
2. How do I set up to use TDM slave mode?
…