Part Number: TLV320AIC3120 Hi I'm Jieun,
I have some questions about TLV320AIC3120 Audio CODEC.
In datasheet, it indicates that the recommended level of inputs is 0.707Vrms(@AVDD=3.3V, single-ended).
I was wondering if I could know Line input and…
Part Number: TLV320AIC3120 Hello,
Does the TLV320AIC3120 need to be given an external clock through the MCLK pin or is there an internal clock we can use?
Thanks.
Part Number: TLV320AIC3120 Hi,
I a m looking for a component for an audio application requiring Noise reduction and Echo cancellation for 1 channel.
Within the miniDSP family I have found the TLV320AIC3120 which seems to be the ideal and cheaper solution…
Part Number: TLV320AIC3120 Hello,
We have the TLV320AIC3120 in a product we've prototyped. We're working on getting the clocks configured correctly since the part is no longer on the eval board. On the eval board, BCLK and WCLK are provided through…
Part Number: TLV320AIC3120 Hi,
My customer requests implementing a howling or echo cancellation function on the miniDSP of TLV320AIC3120.
Has AIC3120 ever implemented a howling or echo cancellation function? If not, do you think that the implementation…
Part Number: TLV320AIC3120 Hello,
The datasheet mentions that the supplies for the part should be sequenced in a particular order in section 7.3.1.
Later in the datasheet, in section 9, it says that the part has been designed to be extremely tolerant…
Hi Andrew,
It's looking like the microcontroller we selected isn't going to have enough spare memory to store our configuration on top of the other code we're running, so we need to use an onboard EEPROM. The user guide for the TLV320AIC3120…
Part Number: TLV320AIC3120 Hello - We are using the CODEC ( TLV320AIC3120) in a battery powered product consisting of the CODEC, microphone, speaker and host processor. We would like to use the ATTINY84 has the host processor and I would like to know if…
Part Number: TLV320AIC3120 Hi,
We are using TLV320AIC3120 codec in our board. I have a doubts regarding Headset detection/ mic det functionality.
In datasheet, it is mentioned that I have to configure Page 0 register 67(0x43). Consider I'm using standard…
Part Number: TLV320AIC3120 Hi team,
My customer has trouble of noise clipping(cracked) when playing back sound recorded with the TLV320AIC3120's microphone input.
They consider to adjust following register setting for recording.
Is there any suggestion…