Part Number: TLV320AIC3120 Dear TI members,
TLV320AIC3120 can support below master mode ?
MCLK receive and the output BCLK / WS to host processor .
I can't find this configuration in your Application report (SLAA469A)
Best regards,
Part Number: TLV320AIC3120 Hi sir/ madam,
In our custom project, we are interfacing codec (TLV320AIC3120IRHBT) to Vocoder(AMBE-4020 Full-Duplex BGA) i.e., digital audio data is sent through I2S to vocoder.
It is said that in codec, mono DAC inputs the…
Part Number: TLV320AIC3120 Dear team,
I am using the TLV320AIC3120 AUDIO CODEC, and I would like to inquire about the settings for the MIC1LP.
Using Mono Mic (Low Impedance), I set the resistor to RIN=10kohm to use the maximum gain based on Single Ended…
Part Number: TLV320AIC3120 Hi,
I am configuring CODEC to generate a beep to the speaker output, but I am unable to generate it. Please find the register_configurations.tcl being done for CODEC with inline comments.
Divided the configurations in to three…
Part Number: TLV320AIC3120 Hello Expert,
Could you tell me what the impedance (this pin to ground) or status (Floating, Pull-down, etc) of DIN pin is when TLV320AIC3120 is not powered?
Because this pin is connected to the SoC and pulled-up (10kohm through…
Part Number: TLV320AIC3120 Hi,
I am planning to interface ESP32 with TLV320AIC3120 Codec module. There are Linux device drivers available in the product page.
Is there Arduino supported library available?
If yes, Please point me there
if no, Please…
Part Number: TLV320AIC3120
Hi,
Greetings!!!
I am planning to implement a usecase where I need to live stream audio data to server.
1) Is it possible to stream live audio data from Microphone using the Codec TLV320AIC3120?
If yes, In what formal do host…
Part Number: TLV320AIC3120 Hi,
The data sheet says there are two modes
1) I2S
2) DSP
whats the difference between these two?
Does that mean we can not use the features of DSP when we are interfacing the codec to host controller through I2S interface…