Part Number: TLV320DAC3100 Hi
I am trying to play a beep sound for this TI TLV320DAC3100 Audio DAC chip via i2c from my Nordic 5340 MCU.
Followed the PC control software i2c initialization script sequence that I could play a beep (and output to the connected…
Part Number: TLV320DAC3100 Hi team,
Could you suggest the best processing block for my customer's use case?
They are going to use TLV320DAC3100 in a measurement equipment and play some information sounds not music.
The sampling frequency is 22.05kHz…
Part Number: TLV320DAC3100 Hi team,
TLV320DAC3100 seems to support TDM operations. But I noticed there isn't regarding registers to set TDM mode. Could you let me know how to set the device as TDM mode?
And If you had a sample .c codes that anything…
Part Number: TLV320DAC3100 Hi there,
We've selected the TLV320DAC3100 as possible succesor of one of our previously selected I2S amplifiers as its features are so extensive. A little background information; we're using an nRF52840 as I2S master which…
Part Number: TLV320DAC3100 Hello Team,
I am using TLV320DAC3100 Audio amplifier in my project. I have given below power on sequence in my board 1. SPKVDD, IOVDD and AVDD ( 3.3V) voltages are given simultaneously without any delay 2. DVDD(1.8V) has been given…
Part Number: TLV320DAC3100 Hi Ti team
Can you please review the attached schematic?
I need to connect to my PCB external speaker via 3.5mm jack.
The CPU on the board is NXP iMX8.
I don't need any microphone or analog input, only the interface between…
Part Number: TLV320DAC3100 Other Parts Discussed in Thread: LM49450 Hi I was searching for the Code example or driver for TLV320DAC3100 that i can use with arm cortex M controllers. So far i was able to get linux drivers only. that is complex to understand…
Part Number: TLV320DAC3100 Hello,
What is the meaning of Rise time / Fall time in slave mode of TLV320DAC3100IRHBT?
The datasheet says 4ns(max).
is it NG if the rise time is faster than 4ns?
The I2S tr/tf output specification on the microcontroller side…
Hi Deeksha,
I've been testing some of these sampling rates and they seem to work OK on my side. There are a few things I'd like to double check:
Is your MCLK 26MHz for all cases?
When you say you test 8kHz, 44kHz and 48kHz, you mean these are…
Part Number: TLV320DAC3100 Hi team,
There is a 320kHz output signal from SPKM & SPKP when TLV320DAC3100 works. Is it ok to configure the device outputs at a certain DC level? Customer wants to make audio lead-off detection through this way.
Do you have…