Part Number: TLV320DAC3203EVM-K Using TLV320DAC3203EVM-K connected to the USB-MODEVM, I can setup the device using I2C
P12-20 SDA
P12-18 Ground
P12-16 SCL
and it functions correctly. If I disconnect the USB-MODEVM and add the connections as follows:
…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 In the TLV320DAC3203 Applications Reference Guide, I see 2 issues.
https://www.ti.com/lit/ug/slau434a/slau434a.pdf?ts=1680509518115&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 1. Set all switches, jumpers to default positions.( see pics on customer support ticket CS1354574)
2. Ran Beep test - works as expected.
3. Put music CD in PC and played thru…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 , Hi Team,
When testing TLV320DAC3203 Class-D mode, Sine wave signal input through INL/INR, and measure output HPL/HPR is no signal output. When the setting is change to Class-AB…
Part Number: TLV320DAC3203 Hi, teams,
TLV320DAC3203EVM and mother board are default setting, and use USB cable connect board and computer,
On the USB-MODEVM, LEDs D3, D4, D5, and D7 illuminate
D2 on the USB-MODEVM illuminates, indicating that the firmware…
Part Number: TLV320DAC3203EVM-K
Hi Team, My customer considers to use TLV320DAC3203EVM-K + USB-MODEVM. He wants to evaluate it with external I2S signals from another board. Is it possible? I would like to know hardware settings to achieve it. Best Regards, …
Other Parts Discussed in Thread: TLV320DAC3203EVM-K Hi,
Could someone help me to locate the Gerber file for this EVM (TLV320DAC3203EVM-K)?
Thanks.
Regards,
Deejay
Hi,
I just tested your PLL case with the help of our TLV320DAC3203EVM-K and it is working correctly.
I'm using MCLK = 25.576MHz, WCLK = 48KHz, BCLK = 3.072MHz. Even if I modify the clocks, I can still hear audio from the DAC outputs.
Have you tried…
Hello,
Here is a very similar E2E thread that may also be helpful. Please install in "Administrator" mode and also run it in that mode as well and if that doesn't work try restarting the SW.
https://e2e.ti.com/support/audio/f/6/t/864658…
Newer EVMs (~2007+)
The EVM User Guides for the devices below have been updated to include instructions on how to use these EVMs under Windows 7. Click a device, open the User Guide and search "Windows 7".
For the devices below, the EVM firmware…