Part Number: TDC7201 Other Parts Discussed in Thread: TLV3601 , Hi,
Customer question:
Is impedance matching required between the output of the comparator (TLV3601) and the input STOP2 pin of TDC7201?
Thanks,
Tyler
Jimmy,
We have many devices in high speed niche. Can you share any details in your system and comparator requirements besides 5V?
For 5V, we have TLV3201 (40ns) and TLV3501 (4.5ns), TLV3601/2/3 (2.5ns), TLV3604/5 (800ps, LVDS) and TLV3801/11 (225 ps,…
Part Number: TLV3601EVM Other Parts Discussed in Thread: TLV3601 Good morning,
I am going to purchase a TLV3601/3603 evaluation module, and want to clarify if the EVM comes populated with all components. Most of the images appear to show an unpopulated…
Other Parts Discussed in Thread: SN74AUC1GU04 , TLV3601 We have a laser trigger pulse which has 250mV amplitude and 2 ns pulse width. We would like to seek a simple solution to shape the laser pulse to 3.3 LVCMOS level and at least 30ns pulse width. Any…
Hi Raj,
Sorry yes you're right. It will be limited by the toggle frequency and pulse width of the signal going into the TLV3601. Unfortunately we do not have a faster single ended output device that could handle that high of speed.
Hello Gustavo,
Sorry for the delay.
We have many new high speed options. What is the minimum pulse width of your signal?
We have options with speeds from 40ns to 2.5ns, with conventional or LVDS outputs.
See the TLV3201, TLV3501 and TLV3601 families. …
Part Number: TLV3605 Other Parts Discussed in Thread: TLV3801 , TLV3601 Hi,
I would like to check that
1) Can TLV3605 accepts negative voltage (For example -1.7V) at its VEE pin?
2) Do the LVDS output refers to the VEE pin as its ground reference? If…
Hello Bisso,
Do you need the shutdown? Does it need to be in the same pinout? Can you use a dual? Any package preferences? Prefer low cost or better performance?
There are several options. See out the LMV7219, TLV3201, TLV3501, TLV3601. There is also…
Hi Alex,
Are you looking to operate split supply to allow for the common mode input voltage to go negative? Keep in the mind the output will now swing negative VEE to VCC. With that speed, we have TLV3601 and TLV3501.
If you would like to go split supply…
Patrick,
I am still figuring out the issue with TLV3603 which may take some time. As a temporary fix, I replaced it with the TLV3601 (same device without the LE/HYS pin) and I am having it emulate a 35mV hysteresis just like how you're setting up the…