Part Number: TLV3602 Other Parts Discussed in Thread: TLV1871 , TL3016 , TL3116 Hello,
As a replacement for the MAX901 comparator, you are recommending the TLV3602. This component is not equivalent. I would like to power the comparator between +5.2V…
Part Number: TLV3602 Hello,
My customer is looking for a low-cost replacement for the LT1715.
Please recommend the best low-cost replacement for LT1715.
Thank you.
Part Number: TLV3602 Other Parts Discussed in Thread: TLV3601 , TLV3601-Q1 Hi Teams,
My customer is looking for a high-speed comparator. The requirements are as follows: 1.Power supply 1.8V~3.3V 2.Input signal frequency ≥ 200MHz 3.Low end-to-end transmission…
Part Number: TLV3602-Q1 Other Parts Discussed in Thread: LMG2100R044 , TLV3602 , TINA-TI Hi expert,
My customer is using LMG2100R044 as power stage. This power stage needs complementary PWM, but the controller can only generate 1 PWM.
I recommended…
Part Number: TLV3602-Q1 The TLV360x datasheet states that the inputs can be driven up to 200mV beyond either of the rails. The datasheet also states "to avoid damaging the inputs when exceeding the recommended input voltage range, an external resistor…
Part Number: TLV3602-Q1 Other Parts Discussed in Thread: TLV3602 Dear expert,
According to below table in datasheet, TLV3602 output current is 10mA(min) for VCC = 2.4 to 5.5V , right?
Part Number: TLV761 Other Parts Discussed in Thread: TLV3601 , TLV3602 Hello,
I am looking for reliability data (MTBF or FIT) for the following part that is currently in use: TLV76136DCYR On the estimator tool it shows a FIT of 0.1 but I would like…
Part Number: TLV3602EVM Other Parts Discussed in Thread: TLV3602 Hi,
I'm using the TLV3602EVM as the comparator stage in an application, and I'm seeing an output LOW level that is consistently elevated well above the datasheet's specified VOL. I want…
Part Number: TLV3604 Other Parts Discussed in Thread: TDC7200 , , TLV3502 , TLV3501 , TLV3511 , TLV3512 , TLV3601 , TLV3602 The output of this is differential. There are two outputs here. For my application, I want to use a single output, and connect…
Part Number: LM361 Other Parts Discussed in Thread: TL3016 , TL712 , , TLV3602 , TLV3502 Hello,
I am working on to redesign a legacy PCB with modern components. However, I have been having trouble finsding a "drop-in" (more in terms of function) replacement…