Part Number: TLV62065 Hi team,
I tested the bode plot without Cff as below. However I can’t figure out how the inside compensation works.
Could you please tell me the inside loop compensation circuit ? Is this the third or second compensation? Thank…
Part Number: TLV62065 Other Parts Discussed in Thread: TLV62080 , , TLV62569 , TLV62568 Hi Sir
My customer currently use TLV62065DSGR/TLV62080DSGR/TPS81256SIPR .
But they need know if TI have TLV62065DSGR/TLV62080DSGR/TPS81256SIPR next generation product? …
Part Number: TLV62065 Other Parts Discussed in Thread: , TPS62097 Hi,
Thermal information of TLV62065 is different of TLV62065-Q1's as follows.
And TLV62065-Q1's is newer(and better) than TLV62065.
Can we refer the thermal information of TLV62065…
Part Number: TLV62065 Other Parts Discussed in Thread: TPS62097 , TLV62085 , TLV62084A , TLV62569 Hi,
My customers need to set the output voltage of TLV 62065 to 1.1 V (≤ ± 3%).
They are referring to Equation 2 of the data sheet to calculate the…
Part Number: TLV62065-Q1 Other Parts Discussed in Thread: TLV62065
Our customer is considering to use TLV62065-Q1.
They found about 100kHz oscillation at output in PWM mode.
I attached thier circuit and waveform.
Please let us know why 100kHz oscillation…
Other Parts Discussed in Thread: TLV62065-Q1 , TLV62065 Our customer consider to use TLV62065-Q1.
They get data of Phase margin,Gain margin.Please see attached.
TLV62065-Q1 Phase margin_Gain margin.pptx
Power save mode :Phase margin:41.7deg,Gain margin…
Other Parts Discussed in Thread: TLV62065-Q1 Hi Team,
I would like to use the TLV62065-Q1 to drive a load with the following conditions:
Vin: 5V
Vout: 3V3
Iout: 305mA
load capacitance: 95uF
Will the TLV62065-Q1 be able to drive a load with that high of…
Other Parts Discussed in Thread: TLV62065-Q1 , TLV620612-Q1 Dear, Sir.
My customer is considering to use TLV62065-Q1 as Vin=5V, Vout=1.1v converter.
The minimum on-time is not defined on the datasheet & I can't make decision to refer other thread.…
Other Parts Discussed in Thread: TLV62065-Q1 Our customer consider to use TLV62065-Q1.
Please let us know following values of this device.
1. Minimum On-Time (min,typ,max)
2.tSTART(Startup time) (min,max) typ is 500us in datasheet P6
3.tRAMP (min…