Part Number: TLV702-Q1 Hi,
The PN is TLV70230QDSERQ1;
We use TLV70230QDSERQ1, input 3.3V or 4V, measured output is 2V, EN is 2.8V, how many inputs should be set to get stable 3V / 300mA, does the circuit need to be adjusted? How to adjust?
Is there a…
Part Number: TLV702-Q1 Hello,
We are using the TLV70215 and looking at the output capacitor ESR requirements. The datasheet states the equivalent ESR should be less than 200mOhm.
We have a 10V, 1uF Multi-Layer Ceramic Capacitors (MLCC) on the output as…
Part Number: TLV702-Q1 Hi,
Max output current is estimated 305mA on my customer's circuit.
Should I promote TLV702-Q1 though output current may over recommended condition?
My customer requirements are follows;
- VIN=3V~3.6V
- VOUT=1.25V or 1.3V
-…
Part Number: TLV702-Q1 Hi
Is the LDO output able to maintain the 3.3V if the output is series with a voltage source in this case? See above picture for reference. Thanks!
Part Number: TLV702-Q1 Other Parts Discussed in Thread: LP5912 ,
Hi Team,
I check that TLV70233 doesn't have reverser protection function as LP5912.
But customer would like to know how much current could the internal body diode could tolerate when…
Part Number: LP5907-Q1 Other Parts Discussed in Thread: TLV702 , TLV700 Hi team,
why there is maximum capacitor limited for LP5907-Q1? if the maximum capacitor is larger than 10uF, what will happen? It seems there is no such limit in other parts.
thanks…
Other Parts Discussed in Thread: OPA1662 , OPA1664 , TPS22919 , TPS22960 , TLV702 , TLV7021 , TLV702-Q1 Hello,
I recently designed a PCB using some TI components. I wasted to perform a signal and power integrity analysis of the PCB. I needed the IBIS models…
Mitchell,
I'd say that the LP5907-Q1 has better noise characteristics and load response. The PSRR is pretty similar between the two. If noise or transient response aren't a concern, then TLV702-Q1 could work.
~ Aaron
Hi Ryan,
The TLV702-Q1 WSON package(1.5mmx1.5mm) is not same package as TLV733P-Q1 WSON package(2mmx2mm).
Do you have other suggestion?
Thanks,
Patrick
Hi Ian,
For higher PSRR please consider TLV702-Q1; however, it is important to note that these devices are not pin to pin compatible.
For part suggestions, keep in mind that the more information you can give us about how you are planning to use the…