Part Number: TLV710-Q1 Tool/software: Hi team,
Does the TLV7103318QDSERQ1 have an internal pull-up or pull-down resistor on the EN pin? What does the Q in the part number mean?
Best Regards,
Jade Lan
Part Number: TLV710-Q1 Hi Team,
We have used TLV7103318QDSERQ1 for SD card supply for our board, during the prototype phase the board was working with SD card booting. After some 100 board production we faced the issue that showing 1.1V instead of 1…
Part Number: TLV710-Q1 Hi team:
Can the TLV7103318QDSERQ1 output1 and output2 be combined? It appears to be mirrored in block diagram. Input 5V, output1&output2 for 80mA
thanks.
Part Number: TLV710-Q1 Other Parts Discussed in Thread: TLV710 Hi Team,
We have used TLV7103318QDSERQ1 for SD card supply for our board, during the prototype phase the board was working with SD card booting. After some 100 board production we faced…
Part Number: TLV710-Q1 Hi,
In the Jacinto7 EVM design, the 1.8V and 3.3V output of TLV7103318 are short with 0ohm resistors as shown in the figure below. And here is description that if we want to achieve 3.3V output, the EN1 and EN2 should be both…
Hi Zoe,
Both outputs are capable of a load current of 200 mA at the same time; however, you will need to also consider the thermal performance.
You can use the Rthetaja from the Thermal Information table for a first pass check on your thermal performance…
Part Number: LP3996 Other Parts Discussed in Thread: TLV710-Q1 , , TLV751 Hi,
Could you please recommend an alternative device for LP3996 and TLV710-Q1 that has a lower Iq? I can't find any other device than those devices I have mentioned. My required…
Part Number: J721S2XSOMXEVM Tool/software: Hi support team,
The attachment is the Power Estimation we filled out. Please help to review, thanks.
Another question is whether the TDA4AL EVM has high-temperature testing?
Specifically, at ambient temperatures…
Ramgopal,
Your assessment of the bulk decoupling required is correct. You must calculate the required amount and validate it. The Hardware Design Guide (SPRABI2) discusses this calculation.
This bulk capacitance will affect the control loop on the…