Part Number: TLV742P Hi, teams
Absolute maximum ratings of EN pin is -0.3 ~ 6 V, that is no dependence on Vin.
This means that is no problem applying voltage to EN pin without Vin?
In our system, above condition occurs while power-on sequence.
Best…
Part Number: TLV742P
Hi,
I am simulating about a circuit using LTSPICE. TLV74218P and TPS22914C netlists were imported into LTSPICE. Looking at the simulation result, V(out) is 2.607V,but correct value should be 3.3V(The output of TLV74218P should be…
Part Number: TLV742P Other Parts Discussed in Thread: TPS22914 Hi, Team
I designed power mux circuits with TPS22914C and TLV742P like figure.
Circuits are operated as the following: 1. Enable TPS22914C and Vout rises to Vout_SW 2. Enable TLV742P. 3. Optionally…
Part Number: TLV742P Hi,
I am thinking about a circuit where a voltage higher than Vout and lower than Vin is applied to Vout when the EN pin of the TLV742P is High or Low.
Can the IC operate without problems after removing the applied voltage?
Thank…
Part Number: TLV742P Why the package dimension are not in the datasheet?
When I try downloading package CAD file is in not readable format by any standard viewer I have (no PDF, no eDrawing and other)
How I can get the package dimension and why they are…
Part Number: TLV742P Hi team,
The datasheet shows a startup time value in a condition of Cout=1uF and Iout=150mA. How much does the startup time varies when Cout and Iout are changed? If you have simulation result or measurement data which describes startup…
Part Number: TLV742P Other Parts Discussed in Thread: TLV755P The TLV742P (and TLV755P) datasheets state "PSRR and transient response degrade when (VIN – VOUT) approaches dropout." I'm not sure what "approaches" means. I…
Part Number: TLV757P
I am considering using a TLV75733PDRVR LDO to drop 4V to 3.3V while driving up to 1A, thus needing to dissipate around 0.7 watts. Would an additional heat sink be required in this situation, assuming the PCB provides a large copper…