Part Number: TLV751 Hi team,
I would like to ask a question about TLV75101PDSQR. As shown in the picture below, I connected both OUT1 and OUT2 channels of TLV751 to output "FPGA_HSSTAVCCPLL_1.2V" at the same time. What I want to ask is whether I can…
Part Number: TLV751 Hello team,
I would like to ask a question about TLV75101PDSQR. As shown in the picture below, I connected both OUT1 and OUT2 channels of TLV751 to output "FPGA_HSSTAVCCPLL_1.2V" at the same time. What I want to ask is whether I can…
Part Number: TLV751 Dear Team,
we wan to use TLV751180330PDSQR for 1.8V and 3.3V
Vin = 3.4V
Vout1=1.8V Iout1= 20mA
Vout2=3.3V Iout_max=88mA Iout_typ=72mA
Would you recommend TLV751180330PDSQR for this application ( regarding dropout voltage )?
Would…
Part Number: TLV751 Hi team,
I check that The TLV751 is a dual, adjustable, 500-mA low drop out (LDO) regulator. But I am not sure if 2 channel can provide 500mA at the same time, especially when their voltage between the input and output is large. Could…
Part Number: TLV751 Hi team,
In datasheet, the output voltage fixed option is 0.65V to 5.0V.
How we can reach the output fixed 0.65V product page?
And if we use the adjustable option set 0.55V output, is it correct that set FBx pin connect to OUTx directly…
Part Number: TLV751 Other Parts Discussed in Thread: TLV755P , TLV758P , TPS7A90 Hi team,
My name is Simeon Aleksandrov, I am an FAE intern at TI BeNeLux.
We are searching for an LDO for 5V0 Vin to Vout 3V3 @ 500mA. Key requirements:
High PSSR
Good thermal…
Part Number: TLV751 From the datasheet the enable signals (pin3 and pin5) of the TLV751180330PDSQR are both active high.
I am driving the enable signal with an push-pull output of a microcontroller.
I would like to know if the input voltage (pin 9 and…