Part Number: TMAG5173-Q1 Tool/software: Hello,
We want to make hall effect push buttons with s afety compliant . I have tried this sensor and my measurements are:
-09 mT when not pressed
-27 mT when pressed
Is it suitable for push button application? …
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5173EVM Tool/software: Hi,
I am using this sensor for angle measurement in rotary application for XY.
I am using example code. I am getting weird result for angle like in these pictures.
…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5170 Tool/software: Hello! I'm seraching for a magnetic sensor with high analog bandwidth for measuring flux of ~15 ... 100mT(or less) @ up to ~8kHz and with SPI or I2C. I want to measure…
Part Number: TMAG5173-Q1 Summary
Our use of the sensor involves reading and triggering via I2C conversions for X-axis and Temperature in 16-bit mode with CRC enabled. In our testing we simulated a power loss by powering off/on the sensor. We hoped to…
Part Number: TMAG5173-Q1 Sensor 177 and sensor 180 share an I2C Bus. The rotation count represents a conversion read/trigger from the sensors at 780Hz. CONV represents a 0 for RESULT_STATUS in CONV_STATUS register, and CRC indicates a CRC error on the…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: TMAG5170 , , TMAG5170-Q1 Hi,
435 / 5,000
I am preparing to use a 3D Hall effect sensor = comparing TMAG5173 and TMAG5170 there are a few differences: 5170: SPI, 8…
Part Number: TMAG5173-Q1 Hi Team,
My customer used TMAG5173-Q1 to develop the HMI. I'm not familiar with the part.
Do we need to do initial setting for 0h-Bh register before getting result from 10h-1Ch?I
If so, do we have initial setting script can…
Part Number: TMAG5173-Q1 Other Parts Discussed in Thread: MSP430FR2422 I am using an MSP430FR2422 processor and have a prototype PCB with the sensor, processor, and JTAG emulator. I can get readings using the I2C to trigger the conversion and the sensor…
Part Number: TMAG5173-Q1 Hi,
I am working on a tolerance estimation and I am using the TMAG5173A2 Hall-Effect Sensors. For this purpose, I would like to estimate the sensitivity error and the offset as a distribution function.
Therefore my question: How…
Part Number: TMAG5173-Q1 Hello,
as i am working on ultra low consumption design, i would like to understand well the of the test description column corresponding to the "Under voltage threshold at VCC" line. That is to say "Internal parameter (OTP option…