Hi Misael,
The following is my response, please help, thank you.
-
-
-
McASP supports mono audio only in a 2-TDM slot fashion. That is, one slot (the first one) carries the audio data, and the other slot is zero-padded. McASP doesn't support…
Part Number: J721EXCPXEVM Tool/software: Hi,
I am trying to execute rpmsg_char_simple application with different remote proc ids, but they all seem to fail.
It throws the following errors,
root@j721s2-evm:~# rpmsg_char_simple -r0 _rpmsg_char_find_ctrldev…
Part Number: CC3220SF-LAUNCHXL Tool/software: Code Composer Studio Hi team
My customer uses cc3220sf launchpad rev-a, SDK version: simplelink_cc32xx_sdk_2_30_00_05
He followed the below link,but got failed
http://software-dl.ti.com/ecs/SIMPLELINK_CC3220_SDK…
Hi Justin,
Thanks for your quick reply! I will try the LRPD demo.
I've read the 0753.swru546c----mmWaveICBoost and Antenna Module.pdf , in which it mentioned " IWR6843ISK / IWR6843ISK-ODS (deprecated)". I want to ask what the "deprecated" means, …
Hi Khushboo, Sure. Attaching the zip here.
omapboot.txt.txt
Just rename it to omapboot.tar and then just do tar -cvf omapboot.tar
Best Regards, Keerthy
Badri,
I assume that you are using the bq34z100EVM. Make sure that the jumpers are in the proper locations. The J5 jumpers should be in the >5V locations and the J2 jumper should be in the 16V location. If you have already attached the cells with the…
Paul,
First, hoping the end-user realizes this is an obsolete device, NRND.
Next, if the clock either loses accuracy, or does not retain clock information, then the internal battery has been discharged.
I have attached the BQ4850Y Product Specification…
Hai,
I've attached the user guide here, it looks like there is a mux on the EVM that handles the loopback. This is a really old EVM, and I don't have a Windows XP machine that runs the GUI anymore, so my ability to recreate your setup is limited.
…