Part Number: TMCS1100 Other Parts Discussed in Thread: TINA-TI Hi E2E,
Our customer was simulating the TINA TI and Pspice models of TMCS1100A4 and it has different output as seen in the attached figure.
The TINA-TI shows the output value according to…
Part Number: TMCS1100-Q1 Other Parts Discussed in Thread: TMCS1100 Hello, I've been looking at the TMCS1100 series of current sense ICs and the sensitivity of the A4 version would give better measurement resolution compared to the A3 version.
However…
Part Number: TMCS1100 Dear sir,
We are planning to use TMCS1100A1 Current sensor IC in our product. Is TMCS1100A1 IC UL 1577 and IEC/CB 62368-1 Certified?
Thanks
kadam
Part Number: TMCS1100 Hi, Team,
A relay is installed near the TMCS110 in the application. Since the relay may have a magnetic field, there is concern which can affect the current sensor.
How far is it recommended to keep the two apart? If you have any reference…
Part Number: TMCS1100-Q1 Other Parts Discussed in Thread: TMCS1100 , DRV425 Hi team,
My customer wants to use TMCS1100 in their BMS application but their current is 800A max, they are asking if they can connect multiple sense resistors in parallel with…
Part Number: TMCS1100 Other Parts Discussed in Thread: TINA-TI The current inputs IN + and IN- appear to be inversed on the TMCS1100 simulation model. When the current increases, the output voltage decreases contrary to what Figure 46 shows in the datasheet…
Part Number: TMCS1100
Hello,
We are working on a project where were are using TMCS1100A3 current sensor to measure the motor current to control the motor. We want to run this motor continuously for extended hours. The motor runs for a few hours and stops…
Part Number: TMCS1100 Hi,
The PDF datasheet download link at the top of the TMSC1100 product page at https://www.ti.com/product/TMCS1100 doesn't seem to work. It doenloads a broken or empty PDF which won't display either in browser or in an external…
Part Number: TMCS1100 Dear TI support team,
I would like to use the TMCS1100A4B for an application where I have to sense -1A<I<1A. I've planned to set a Vref of 1.5V, so I'm expecting to have an output voltage that swing from 1.1V to 1.9V. Considering…
Part Number: TMCS1100 Hello, I have a small question on continuous current range. As the max continuous current of TMCS1100 is about 20A, could two chips of TMCS1100 be in parallel connection, then the max measurable current will be 40A?