Part Number: TMCS1100 Hello,
According to the datasheet, all safety-related certifications are "planned" as belows.
Safety related certifications (planned) – UL 1577 Component Recognition Program – IEC/CB 62368-1
When will you get…
Hello,
I forward my question to you on the advice of: Jonathan Navor Texas Instruments | Customer Support Center
I bought an evaluation board through mouser. When I connect the A3 evaluation module (power only and no current through the sensor), I already…
Part Number: TMCS1100 Hi Team,
Some quick questions.
When an overcurrent occurs in my customer's circuit, there is a possibility that a maximum of 60A(10ms single pulse) current may flow through the sensing part of the current sensor.
1. What happens…
Part Number: TMCS1100 Hello team,
Is DTI at 60um same with the thick of the stuff for isolation ?
And TMCS is applied to the isolation of IEC-J60950 or reinforced isolation ?
Thank you and best regards,
Michiaki
Part Number: TMCS1100 Dear team,
I see we had not add capacitor to Vout and Vref in the application design in datasheet, customer wonder if no capacitor will effect the response time and EMC test. Would you give suggestion that what value capacitor should…
Part Number: TMCS1100 I notice from the data sheet that the absolute maximum values for Vout are (Gnd - 0.3V) to (Vs + 0.3V).
What isn't clear is whether that would apply to a voltage applied outside the IC or whether it could also apply to an internally…
Part Number: TMCS1100 Other Parts Discussed in Thread: TMCS1101 Hi
Can TI TMCS1100 be replaced ACEINNA MCA1101-50-5?
Or there are other ICs that can replace, thanks.
6020-1102-01 RevE_MCA1101_20190627.pdf
Regards
Rock
Part Number: TMCS1100 Hi Sirs,
My customer would like to know the TMCS1100's Hall-effect current sensor is or not support to reduce magnetically induced interference, same as Allegro/ACS725 shown as below red block.
If any, please advise. Thanks…
Part Number: TMCS1100 Hi,
A "clean" current of 500mA (green) leads to the following output signal of the TMCS100 (yellow). Scope_2.bmp in the attachment. The 100mV jump corresponds to a current jump of 250mA, and this is seen on the Oszi. The…
Part Number: TMCS1100 Hi,
I heard that TMCS1100 was supposed to release in the end of March 2020, but I found it was still "Preview" status on TI Website.
is it possible to share the current RTM schedule with me?
Sincerely
Go