Part Number: TMP114 Other Parts Discussed in Thread: MSP430F5528 , USB2ANY , TMP144 , TMP144EVM , BOOSTXL-TMP107 , TMP107 , TMP104 Hello, do you have MCU SW or CCS project which read out the TMP114. Also the EVM project would work.
Regards, Holger
Hi Itoh-san,
TMP144 and TMP104 uses only one command byte where TMP107 uses two.
The devices respond with two bytes each in TMP144 (same as TMP107,) or one byte each in TMP104.
The delay between responses is 1 baud in TMP104/144 as opposed to 1.5 baud…
Part Number: TMP103 Other Parts Discussed in Thread: TCA9548A , TMP1075 , TMP144 , TMP104 Hi,
What's the input capacitance for the I2C pins on the TMP103? Any concerns with attaching 6+ TMP103 onto the same bus?
Thanks,
Peter
Hi Revenant,
I'll let Daniel answer your thermistor question, but you might consider using a daisy-chain product like TMP107 or TMP104 instead. These products use robust UART communication to provide accurate temperature measurements at several nodes…
Other Parts Discussed in Thread: TMP117 , LMT01 , LMT70 , TMP104 , TMP116 1. I need a digital temperature sensor with an accuracy of + 0.1 C. I think only TMP117 meets the requirements. When will this material be mass produced?
The accuracy of the
2. TMP117…
Hi Ren, thanks for explaining. I'm hoping for a true "UART compatible" sensor which to me means you can literally hook it up to a UART port (such as a common USB-UART bridge dongle etc.) The pdf you provided indicates TMP104 can do this directly with…
TMP107 features an SOIC package and one-wire interface, but it is a UART based interface. The unique interface in the TMP107 is able to daisy-chain up to 32 devices using 3 conductor cabling (Power, Ground and Bidirectional Comm.)
TMP104 features a…
Hi Kazuya-san,
1. This is a broader question about statistics and risk. We require at least 30 devices for development and release of our own products. Other companies may have other standards.
2. It typically varies more from manufacturer to manufacturer…
How many nodes do you need?
TMP75 offers 8 pin configurable I2C address options
TMP175 offers 27 pin configurable I2C address options
TMP103 offers 8 orderable I2C address options
TMP104 supports up to 16 devices in a daisy-chain with UART communicat…