Part Number: TMP112 Hi Teams,
The customer is using TMP112 to develop an enterprise grade SSD application and has discovered an issue with one of the ICs. They have requested FA analysis and the current feedback is to ask the application team to help…
Part Number: TMP112 The TMP112 datasheet (SBOS473L – MARCH 2009 – REVISED JULY 2024) section 7.5.3 shows the configuration register.
The lower 4 bits are listed as just 0 without a description.
Should I write 0 to these 4 bits when setting other documented…
Part Number: TMP112 Other Parts Discussed in Thread: TMP102 ,
Do TMP102 and TMP112 support I2C clock stretching? If yes, could you describe how it is implemented internally?
Under what conditions would clock stretching be triggered? For example…
Part Number: TMP112 We are using temperature sensor TMP112AIDRLR on one of our products. Our customer is asking for temperature calibration certificate of the sensor.
Part Number: TMP112-Q1 Other Parts Discussed in Thread: TMP112D , TMP112 Hi Team,
We are using the TMP112AQDRLRQ1 IC in our project, which operates at a maximum supply voltage of 3.6V . However, our controller operates at 5V .
We would like to know…
Part Number: TMP112 Tool/software: On table 6.3 Recommended Operating Conditions in the datasheet for the TMP112 the V+ Supply voltage has a range of 1.4V to 3.6V. But, on the first page of the datasheet it give the accuracy for various versions of the…
Part Number: TMP112 We are using temperature sensor TMP112BIDRLR on one of our products. Our customer is asking for temperature calibration certificate of the sensor. The certificate if essential in the context of the pharmaceutical qualification of the…
Part Number: TMP112-Q1 Hi,
Our customer designed the I2C pull-up for the TMP112-Q1 using 3.3V and a 1k resistor. This configuration appears to slightly exceed the 3mA limit.
When the temperature changes from room temperature to 5°C, one out of ten…
Part Number: TMP112 Hi, For the TMP112 I²C timing spec, the datasheet lists t(HDDAT) (data hold time) as 100–900 ns (as table in Section 6.6). I would like to ask: Is there any risk if t(HDDAT) is below 100 ns? Thanks.
Part Number: TMP112 Hi E2E,
What is the exact test condition of Iq when serial bus is active? I found the comment below from old thread :
Iq in this case includes both the current due to conversions(default - 4Hz case) and the current due to SCL…