Part Number: TMP126-Q1 Application issues of tmp126-q1
We attempted to change the 10K resistor of the string to 1.5K, and communication could be achieved at 4M, but it still couldn't meet the 8M requirement
Is there any solution for the actual demand…
Part Number: RM48L952 Other Parts Discussed in Thread: TMP126-Q1 , , TMP126 Hi,
I am currently evaluating the best way to interface a TMP126-Q1 temperature sensor with the RM48L952.
The TMP126-Q1 uses a 3-wire SPI interface with a bidirectional SIO…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 When reading the TMP126, is the MCU side in the normal four-wire mode (according to your hardware design)?
Part Number: TMP126-Q1 We attempted to change the 10K resistor of the string to 1.5K, and 4M could communicate, but it still couldn't meet the 10M requirement. The actual demand is for a rate of 8M. Are there any other solutions, such as changing the…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP127-Q1 , , TMP127 , TMP126
Tool/software:
Dear team,
Can TMP126-Q1 work with Read-only mode? TMP127-Q1 supports according to the datasheet. We just want higher accuracy than TMP127 but #…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 , TMP127 Tool/software: I'm using the TMP126-Q1 on a board. I have a digital connector that brings over the SPI bus (CLK, MISO, MOSI, CS) from a Raspberry Pi 4B.
I was able to configure…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 , TMP127 Tool/software: Hello, I am using tmp126 with ISO-SPI Communication.(LTC6820)
but i can't read device id.(0x2126)
//SPI-Master #include<SPI.h>
byte masterSend, masterReceive;…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 Tool/software: A follow-up question on the turn around between write and read to/from the TMP126.
The previous tread said that the turn around between write and read is on the first falling…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 When exactly does the SIO pin change from input to output?
The data sheet only says "During a read command the TMP126-Q1 will control the SIO pin after the command word ."
It doesn't state…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 There was an error of the TMP126/TMP126-Q1 DCK package pin out in the initial datasheet release. The results are summarized below:
Jalen