Part Number: TMP139 Hi,
I kindly ask you to help fill in the missing information below:
P/N
Description
Supplier
QTY per Inner Box
Inner Box Dimensions (cm)
Inner Box Gross Weight (kg)
QTY per Outer Box…
Part Number: TMP139 Tool/software: Hi team,
May I know if we prepare IBIS model of I3C of TMP139 to evaluate the signal quality?
Best regards,
Shunsuke Yamamoto
Part Number: TMP139 Hi
We are using tmp139 I3C temperature sensors on board.
We couldn't find unstreamed Linux diver for this device.
Can you pls let us know which linux driver is compatible?
We tried by adding jc42 driver support but no luck…
Part Number: TMP139 Datasheet specified
Vddio = I/O Voltage = 1.0V
Vddpd = Core Voltage = 1.8V
I would like to confirm that these voltages are not reversed - it seems an odd combination, and atypical for what I am used to.
I don't want to…
Part Number: TMP139 Hi Team,
my customer is searching for a temp sensor for DDR5.
spec as below: Vddsp, 1.8V typical, 1.7-1.98V, Vddio 1V typical, 0.95-1.05V, 1MHz I2C and 12.5MHz I3C, 11bit valid data. cover -40~125C. Is TMP139 the most suitable…
Part Number: TMP139 Dear Forum-members,
Can you please let me know how to create tmp139 device node in device tree?
We tried with below option , but no luck
* I3C device with a static I2C address. */
thermal_sensor: sensor@37,39200100000 {
reg…
Part Number: TMP139 Hi experts,
Please kindly help me about the problem :
I have sent (S+0xfc+ack+0x29+T+P) to TMP139 to ender I3C mode. However after I entered I3C, and in I3C Basic Mode Write, no ACK feedback was received after device address sent…