Part Number: TMP235-Q1 Other Parts Discussed in Thread: LM50-Q1 , , LM50 Hi team,
Based on the related thread, it seems that "VOUT short to VDD" is not considered when VDD and VOUT are not on the same side of the package.
LM50-Q1 is a device that…
Part Number: TMP235 Hello Team,
My customer finds that there is a ~400ms -0.45V negative voltage into TMP235's VDD network when the board power up. We are checking the risk about this Voltage. Please help to check the info as below:
What is the…
Part Number: TMP235 hi TI
Tmp235 is greatly affected by PFC circuit operation,The customer uses a 3kW power supply module to measure temperature. As long as the PFC circuit works, the measured value of tmp235 is very unstable and has a large deviation…
Part Number: TMP235 Hi
I want to use thermal couple to do temperature calibration, could you help suggest where should I put it?
On the top of package of TMP235, or just put it between package of TMP235 and PCB?
Part Number: TMP235 Hi,
I am looking at the target applications of TMP235. Can it be used to sense the busbar temperature? I am planning to use a metal clad pcb to place this sensor and then placing this pcb on top of the busbar! please share if you have…
Part Number: TMP235 My team has been using the TMP235A4DCKR for several years but unfortunately we've been unable to source this component easily since 2020. I'm wondering if this component will be manufactured anytime soon and if not is there a replacement…
Part Number: TMP235 Hi team,
My customer wants to know what the TMP235 thermal response time is for 1 °C change in temperature between 25 °C to 60 °C .
Could you please help give an approximate value?
Thanks you!
Regards,
Ivy
…
Part Number: TMS320F28379D Other Parts Discussed in Thread: TMP235 Hi Team,
I am trying to figure out how to connect the temperature sensor TMP235 to my F28379D launchpad.
With the temperature measurement I simply want to detect if the temperature is e…