Part Number: TMP235 Hi,
I am having a problem with TMP235. I am doing some radiated immunity tests on one of my boards and noticed at frequencies between about 330MHz and 600MHz a temperature drift read by the component from 2 to 3°C.
I initially…
Part Number: TMP235-Q1 Dear TI Support team,
could you please help me with one question.
In the TMP235-Q1 sensor datasheet I was unable to find the measures regarding the long-term stability of the sensor?
Should it be supposed, that max accuracy of ±2…
Part Number: TMP235 Other Parts Discussed in Thread: TMP61 , Hello,
What is the difference between TMP 235 and TMP61? Do both have a Die-attach Pad (DAP)? If not, what is the best way to make sure that these devices are thermally coupled to the device which…
Part Number: TMP235 Hello,
I have a quick question about choosing the proper temperature sensor. Is the TMP 235 primarily for sensing ambient temperatures? If I am looking to measure the temperature of a switching device on my pcb, would it be better…
Part Number: TMP235 hi,
we have a question and hope to double-check with you.
Can we put a 0.47uF capacitor between VDD and GND ? the device is TMP235
Thanks
Part Number: TMP235 Other Parts Discussed in Thread: LM50 , , LM50-Q1 , Hi,
Is it true that the only difference between TMP235 and LM50 is the voltage supply range?
The output voltage vs. temperature equation seems to be the same, and the accuracy is almost…
Part Number: TMP235 Other Parts Discussed in Thread: TMP112 , LMT70 , TMP431 , TMP116 Hi,
my customer would like to measure the temperature difference between two points of a sink.
Since TMP235 maximum error is ±1.2C, if they use two TMP235, the temperature…
Part Number: TMP235 Dears,
What is the performance of TMP235 under variable pressure condition? Is there any performance graph showing this characteristics?
Part Number: TMP235-Q1 Hello TI Forum,
My question regard the TMP23X-Q1 is towards where the heat that the component produces directed to? Towards the PCB or towards upwards?
Thanks,
Edan