Part Number: TMP235-Q1 Hi team,
What is difference between AE & AQ? I can't find anything from the datasheet except the "Op Temp" is up to 125C for AQ from the packaging information section. Is this the only difference?
From datasheet…
Part Number: TMP235 hi dear supporting team,
in TMP235 D/S, there is a requirement of total cap load lower than 1000pF, currently customer is using a RC with 1kOhm and 10nF , will it be a problem? tks!
Part Number: TMP235 Dears,
Can you help me to understand the sizing of the output capacitor/filter? Is this mainly for buffering sample and hold circuits of an ADC? I have a fairly slow system, but filtering for lower Hz frequencies, would result in a…
Part Number: TMP235 Other Parts Discussed in Thread: UCD90124A HI team:
our customer find an issue by using TI part TMP235A2DCKR output voltage abnormal at -40℃ again (Vout >1.5V ) ,the failure rate is 5/149=3.36%,the failure DateCode is 1816,
more…
Part Number: TMP235 Other Parts Discussed in Thread: MSP430F5528 , MSP430FR2153 (1) TMP235 has two accuracy levels,
– A2 Level: ±0.5°C (Typical)
– A4 Level: ±1°C (Typical)
(2) • Positive Slope Sensor Gain, Offset (Typical…
Part Number: TMP235-Q1 Dear Team,
could you please tell me where I can find data regarding the Solder Profile including Max. Solder Temperature for TMP235A4DCKR and LMT84QDCKRQ1 ?
Thanks and best regards,
B
Part Number: TMP235 Hi team,
My customer have issue with TMP235A2DCKR. The customer have schematis according to the datasheet. Rfilter is 10 Ohm, Cfilter is 680 pF, Supply voltage is 3.3V.
Device marking - 19L - same as in datasheet.
The output voltage…
Part Number: TMP235 Other Parts Discussed in Thread: TMP236 Hi,
My customer had two questions about TMP235:
1. According to TMP235 datasheet, DCK(S70) package has small size but higher RθJA, not sure if this will influence the temperature accuracy…