Other Parts Discussed in Thread: TMP435 we are using the TMP435 the latest data sheet is from 4/2010 on our chip the mark is : 3A TI DTPI when we try to read the manufacturer code we get 55h like it should but for the device ID its returns 35h insted of…
Other Parts Discussed in Thread: TMP435 , TMP102 , TMP421 , TMP401 Hi,
We are looking for a compatible Linux Device Driver for the TMP435 temperature sensor. We haven't found a compatible one in current upstream Linux kernel, and google didn't return any…
Other Parts Discussed in Thread: TMP435 , DXP Hi,
I am designing a thermal measurement application based on TMP435 device.
I am looking right now for a "cable based" probe to connect on DXN/DXP device pins.
This probe should looks like a:
# 2-wire…
Other Parts Discussed in Thread: TMP435 Hi,
my customer has an internal diode in his SOC and is meassuring with the TMP435 wrong temp. values. According to the supplier of the SOC he circuit to meassure the temp accurately should look as follow using …
Other Parts Discussed in Thread: TMP435 According to the TMP435 datasheet, SDA signal need using an external pull-up resistor as it is an open drain buffer.
But when I use the ibis model (download from TI website) ,the GND_clamp V/I curve of SDA_3 model…
Part Number: TMP464 Other Parts Discussed in Thread: TMP435 , TMP411 , TMP401 , TMP431 , TMP432 , TMP461 , TMP442 , TMP421 , TMP423 , TMP422 , TMP441 Hi Team, Our customer would like to confirm if TMP464 supports Linux kernel and its device tree entry.
Please refer…
Hi SHH,
1. Yes, customer would need to use 432A and 432B on the same bus.
2. Why did customer select TMP432? Do they need Low Beta Correction? We have TMP468 which offers more channels than three TMP432 in one device. Customer can also use six TMP435…
Other Parts Discussed in Thread: TMP435 customer got the ibis model of TMP4xx and found there is no curve and C_comp value for model TERM relate to pin DXP1 and DXN1 of TMP435, pls check it.