Other Parts Discussed in Thread: TMP709 , LM26 , LM57 Hello,
Regarding to the temperature threshold accuracy on TMP709, I have some question.
(1)Can we program the TMP709 temperature threshold by an external 1% resistor at TA>0°C (less than 0°C)?…
Hi,
Thank you for the reply, i think that you should update the bom at 00951 site.
U10 is compatible with TMP300 and TMP709; - your answer is to change to TMP709?
not sure about the heatsink, could you cut off the PIN for assembling? - i am not sure…
Dear Xiuhe -
Please review:
TMP708, TMP709, these devices have the SAME FUNCTIONALITY and PINOUT as the competitors device, but are NOT an exact equivalents
http://www.ti.com/product/TMP708 , http://www.ti.com/product/TMP709
and
LM26 and LM27 these devices…
Part Number: LM5021 Other Parts Discussed in Thread: LM26 , TMP709 Hi, We are checking some protection functions in LM5021. Do LM5021 have over temperature protection? Thanks for your help.
Other Parts Discussed in Thread: TMP708 , TMP709 , LM57 I’m looking for a temperature device where I can attach a resistor to set when a particular temperature has been read.
As an example, if I attach a 10K resistor it will output a low when 65C is…
Hello Mark,
After uploading, in the past, this reference design, we put in the schematic the note that this transformer has to be adapted slightly to the existing PCB (pretty easily I would say: see attached revision E of the schematic, while the online…