Part Number: TMS320F280021 Hi experts,
I am looking at the TMS320F28002x TRM having two questions regarding the eQEP peripheral. As far as I understand, the position counter (QPOSCNT), the eQEP capture timer (QCTMR) and capture period register (QCPRD…
Part Number: TMS320F280021 Hello,
I had a few questions about Figure 7-18 in the TMS320F28002x datasheet.
The figure shows the 20-pin JTAG header connection, and I had 4 questions:
1) what is open drain and where does it connect to?
2) does the 3.3V supply…
Part Number: TMS320F280021 The CAN communication of tms320f280021 is not working,
the code used is from the ti-c2000 ware (can transrecieve)
even if the debugger doesn't show any errors, the pin configured for CAN_TX displays an active high (+3.3 v) throughout…
Part Number: TMS320F280021-Q1 Hi,
I am have an issue reading the raw values from the ADC for voltage measurement I have applied voltage 1.1V on the adc pin, and external VREFHI is 3.3V and VREFLO is grounded
So according to this formula I should I get…
Part Number: TMS320F280021 I am using the TI C2000 to receive data via SCI from another MCU which is 8 bit addressable
The other MCU is sending to TI C2000 data in TWO bytes each is 8 bit and since TI C2000 is 16 bit addressable (the byte is 16 bit) I…
Part Number: TMS320F280021 Other Parts Discussed in Thread: C2000WARE , SYSCONFIG I AM WORKING WITH THE TMS320F280021 MICROCONTROLLER. WHEN COMING WITH CAN COMMUNICATION I USED THE SAMPLE CODE GIVEN IN THE TI C2000 WARE.
THE CODE I TRIED IS "can_ex1_loopback…
Part Number: TMS320F280021 Other Parts Discussed in Thread: C2000WARE I AM FACING SOME DIFFICULTIES IN WRITING A PROGRAM. PLEASE SOMEBODY HELP ME WITH BASIC PROGRAMS
Part Number: TMS320F280021 Hi all,
we have a problem using our designed firmware on a custom standalone board. Our firmware powers up correctly using the JTAG debug emulator, in which we can step through our code.
We are currently using DCSM, so the DCSM…