Part Number: TMS320F280025 Hi team,
I am using F280025 microcontroller in my design.
When I flash my software using CCS, my code works as expected. But after power reset, the software seems to be blank and it is not running at all.
In configuration, I…
Part Number: TMS320F280025
1.Bcakground Introduction:
Operating System: windows 11
Code Composer Studio Version: 12.5.0.00007
Compiler Version:TI v22.6.1.LTS
Output format:eabi(ELF)
Flash uses SEC0 and SEC1, the final program and data is not full for…
Part Number: TMS320F280025 Tool/software: Hello,
I need clarification on the driverlib functions related to selection of negative inputs of comparators in CMPSS:
What is the purpose of the driverlib functions "ASysCtl_selectCMPHNMux(uint16_t select)…
Part Number: TMS320F280025 I want to know the time of different ePWM OST methods
1)GPIO → input X-BAR to TZ directly;
2) GPIO →input X-BAR→ePWM X-BAR→ePWM DC→ePWM OST TZ;
How long does it take to shut off ePWM channles usig the 2…
Part Number: TMS320F280025 Hello support team,
From SPRSP45B I have this info:
If I understand correctly, only F280025C/F280023C have 2 tiles of CLB and the others does not have any CLB.
Could you please confirm that?
Thank your and regards.
Quy
Hi Bo,
Thank you for your observation, I was also able to replicate this issue with CRC_bitReflect and fupdatePI. We're having an active internal discussion with the broader team and will get back to you when we have a conclusion in about a day or so.…
Part Number: TMS320F280025 Hi,
We use the TMS320F280025 for the solar invetere project, and now, we consider to protect t he privacy of the program, we only want to open part of the source program to our cooperating companies,
and the other is hidden that…
Part Number: TMS320F280025 Splitting thread TMS320F280025: The SW issue for TMS320F280025 - C2000 microcontrollers forum
1. For EPWM:
a. The arrangement order of the TBPRD/CMPA/CMPB register related functions within the interrupt will cause EPWM exceptions…
Part Number: TMS320F280025 Other Parts Discussed in Thread: C2000WARE Hello:
I am currently using the routine C:\ti\c2000\C2000Ware_3_03_00_00\driverlib\f28002x\examples\sci\sci_ex2_loopback_interrupts. This parameter is available in loopback mode. Send…