Part Number: TMS320F280049C Champs:
My customer is asking this:
Q1. on the 049 TRM , Section 18.7 / page 1933, there is a Global Load support section.
The question is: When we active the Global load on the Zero point, are the value of (DBRED and…
Hi Quentin,
This error is related to driverlib.lib. Can you confirm that SysConfig now opens?
Quentin Fu said: C:/ti/ccs1270/ccs/eclipse/driverlib/f28p55x/driverlib/ccs/Release/driverlib.lib
This doesn't seem like the correct path it should be pointing…
Part Number: TMS320F280049C Other Parts Discussed in Thread: SEGGER , , CCSTUDIO , C2000-GANG This is the post regarding TMS320F280049C flashing via J-link segger (Part number :8.08.00).
We have TMS320F280049C as per the datasheet J-tag we can use for flashing…
Part Number: TMS320F280049C Other Parts Discussed in Thread: C2000WARE Hello TI Community,
I'm new to interrupts and need some guidance. I've configured my system to receive characters via UART interrupt and send them back to the console via UART transmission…
Part Number: TMS320F280049C Hello,
I am using the TMS320F280049C. In an application three DC motors are current controlled by PWM (Motor1: PWM1 & PWM4 / Motor2: PWM2 & PWM3 / Motor3: PWM6 & PWM7). I want to run all PWMs synchronously with PWM1 defined…
Part Number: TMS320F280049C-Q1 Other Parts Discussed in Thread: PMP41006 Champs:
Q1
My customer has the willing to order this Demo board: PMP41006
https://www.ti.com/lit/ug/tidt253/tidt253.pdf?ts=1712630903528
May we learn Where to order this board? …
Part Number: TMS320F280049C i am making user boot loader for f280049c controller ,in that i will extract bin file using below mentioned method .after that i will receive bin file information byte by byte i will store in internal memory .
in this process…
Part Number: TMS320F280049C Hi,
I want to use the CLA, when the trip zone interrupt occurs. Trip zone occurs cycle by cycle. I use CLA_forceTasks inside the tripzone interrupt ISR. But CLA is not working. Variables in CLA is not changing.
The following…
Hi Gokhan,
Your register view shows the correct values so I'm not sure why you are able to adjust the CMPAHR with the SysConfig but not with bitfield or register writes. Would you be willing to share your project or a subset of your project with us so…