Part Number: TMS320F28022 Hi Team,
Could you tell me the differences ePWM and HRPWM?
What kind of use case each PWM functions will be useful?
REgards,
Takashi Onawa
Part Number: TMS320F28022 Hi team,
Could you tell me Maximum operating frequency with internal oscillator?
Is it possible to achieve 50MHz operation with internal oscillator?
Regards,
Takashi Onawa
Part Number: TMS320F28022 Hi Team,
My customer are using F28022 for automotive application, they have bootloader code and APP code, for each time power on, software will check one flag stored in flash to decide whether jump to the bootloader code or…
Part Number: TMS320F28022 Hi,
in
http://www.ti.com/lit/an/spra963b/spra963b.pdf
the FIT Rate vs. Operating Junction Temperature doesn't show difference between Q100 version and Non-Q100 version for the same package. And the recommended operating…
Part Number: TMS320F28022 Hi Team,
My customer are using ADCINB2/COMP1B/AIO10 for AIO function as output and ADCVINB3 for ADC function, they found that the output voltage of AIO10 will impact the voltage of another pin ADCVINB3 as below show, the peak…
Part Number: TMS320F28022 Tool/software: Code Composer Studio Win7 32 bit, CCS v8, F28022.
This is a problem in CCS6, and I see it is still here in CCS8.
Sooo, adding a bunch of new features, but not fixing bugs. Hmmm, sounds a lot like Ubuntu.
…
Part Number: TMS320F28022 Tool/software: Code Composer Studio I noticed this in CCS 6, and I was kinda hoping CCS8 would have fixed it.
If I edit a .c file and a .h file, then click the "build all" hammer, only the .c file gets auto saved.
Since the…
Part Number: TMS320F28022 Win7 SP1 32bit, Code Composer 6.13, Piccolo 28022 running at 50MHz.
Sometimes, while stepping through my code, I fond some words on the stack do not get changed while under program control.
For example, My stack pointer may…
Part Number: TMS320F28022 Hi Team,
My customer used F28022 as primary PFC controller, and used shadow mode for CMPA register update, and during their products' test, while the bit SHDWAFULL is set to 1, their system THDI is very bad.
Could you kindly…
Part Number: TMS320F28022 Tool/software: Code Composer Studio How do I change the colors of the disassembly window while debugging? Want black background, and green and white text.
Thanks, Mark.