First superset part number has just started production, but there are samples available on TI.com
it typically takes a few months before stock shows up at digikey, etc.
Part Number: TMS320F28379S Dear. Sir/Madam,
I am currently using F28379S 100pin Package, and I have a question regarding the usage of 'Reset' Function.
When using POR Reset, the output from (PWM7A,B / PWM8A,B) maintains LOW Level when Power is…
Part Number: TMS320F28379S Other Parts Discussed in Thread: BOOSTXL-POSMGR , TIDM-02009 Hello,
I'm using the Position manger of TI and using the ExIn to ampliying a sine signal to be use for resolver, but I don't see anything at the output which is ExOut…
Hi,
Just to make sure I completely understand your issue, the output from the SDFM is stable, but you see this issue only after multiplying by certain gain values?
Could you generate another excel file with the gain value that causes your problem? The…
Part Number: TMS320F28379S
Hi all,
I'm using the controller TMS320F28379S for my application I'm using all the 20 Analog inputs, I need to know, how much does the ADC required to given me the result (ADC Conversion time) ?
ADC is triggered using…
Hey Jeremy,
Adding a .syscfg file to a bitfield example such as blinky_with_DCSM won't work, since SysConfig is built on top of driverlib. Could you try the following steps instead?
import the emtpy_bitfield_driverlib_project from the device_support…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Hi All,
I want to use GPIO_SetupPinMux & GPIO_SetupPinOptions and I need to know more about how to use it.
Example : GPIO_SetupPinMux(70, GPIO_MUX_CPU1, 0);// Pin mux option GPIO_SetupPinOptions…
Part Number: TMS320F28379S Other Parts Discussed in Thread: C2000WARE Hello,
In PMSM FOC control application I would like to use overmodulation.
Because of that there will be period when Low-Side Mosfet is not switching (High-Side Mosfet Turned on for…
Part Number: TMS320F28379S What is the lead-time and Life-Cycle of TMS320F28379SPTPS ? Also regarding the technical support.
Is it recommended for a new design?
I don't see Inventory in Suppliers' website.
Regards,
Shai
Part Number: TMS320F28379S Hi,
While checking the data inside the chip through real-time debugging (JTAG) , I found that there was some error (not exactly matched) between the data displayed in Expressions and Graph view and the actual data stored inside…