Part Number: TMS320F28P650DH Tool/software: Hi Experts,
My customer is using the OTA design of putting bootloader and app in one CCS project. In their bootloader, there is a division and "I$$DIV" is called (by compiler), which would cause the bootloader…
Part Number: TMS320F28P650DH Tool/software: Dear champs,
I ask this for customer.
In our LaunchPad design, we use external oscillator and clock buffer in the clock design of C2000 and PHY. In order to save costs, customer wants to use a external crystal…
Part Number: TMS320F28P650DH Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi Team,
For F28P65 has two CPU, and each has a standalone .out, it inconvenient to download two .out on device, so how to combine CPU1's .out and CPU2's .out to one…
Part Number: TMS320F28P650DH Tool/software: Hello,
F28P65x family has an Ethercat controller but I don't need Ethercat, I need Ethernet.
Can I use the controller as an standard Ethernet controller ?
Regards,
Aitor
Part Number: TMS320F28P650DH Tool/software: I added the DCL file to my project and then added the include path. But the project compiles with errors. How do I add the DCL file to an existing project?
the error information as below.
below is the compile…
Part Number: TMS320F28P650DH Tool/software: We use below code to operation flash. After run the flash program function. we can see the flash address have been written successfully. But we read the flash address. CPU2 run to dead status.
what's other…
Part Number: TMS320F28P650DH
Tool/software:
Team,
-I understand from the below thread that CPU2 is always independent from CPU1 (whether or not Lockstep on CPU2 is available on the specific variant). The lockstep feature is specifically between CPU2 and…
Part Number: TMS320F28P650DH
Tool/software:
Hi, can I use the internal ref/bandgap as reference for an external OpAmp? Is it the same for the F28P55?
Regards, Holger
Part Number: TMS320F28P650DH Tool/software: Hi Champs,
I see that peripherals can modify the assigned core via GPIO_setControllerCore(), and FLASH can modify the assigned core via SysCtl_allocateFlashBank. So after the peripherals and FLASH have been…