Part Number: SN74CBTLV3253 Other Parts Discussed in Thread: TMUX1136 , TMUX1119 Do you have 3.3-V, " 2:1 ", 2-channel analog multiplexer which supports Ioff function ? Thanks.
Use the search function . The SN74LVC2G66-Q1 already is the smallest SPST device.
However, the 2:1 SPDT devices TS5A23157, TMUX1072, and TMUX1136 are smaller.
Hi Gust,
The TS5A23159 can be used as a replacement for the FSA2257 and has similar or better performance, however it will not be a pin to pin replacement as the pinouts are different between the devices and package options.
If you need better leakage…
Part Number: TMUX7219-Q1 Other Parts Discussed in Thread: TS5A23159 , TS5A23160 , TMUX1136 e2e,
My application is to connect and disconnect a CAN transmission line and I'm looking for a MUX without body diode.
Requirements:
SPDT -electronic switch…
Part Number: TS5A22364-Q1 Other Parts Discussed in Thread: TMUX1072 , TMUX1136 Hi Team,
Do we have p2p with TS5A22364-Q1, SPDT switch with the same operating temperature and lower capacitance value solution?
Thanks and best regards,
Jamie
Other Parts Discussed in Thread: TMUX1136 , TMUX6136 , TMUX1109 , TMUX1308 , TMUX8108 , MUX36S16 Application Overview:
A very common, but very powerful use of a multiplexer is for applications in which there is a need for more GPIO pins for expanded functionality…
Other Parts Discussed in Thread: TIDA-010019 , SN74CBTLV16292 , TMUX1108 , TMUX1136 , TMUX1308 Hi team,
My customer is looking for MUX for multi-channel temperature sensor, and I’d like to ask your advice.
The system (for 1CH) would be like the one…
Part Number: TS5A3159A Other Parts Discussed in Thread: TMUX1072 , TS5A9411 , TMUX154E , TMUX1136 , TMUX1575 , SN3257-Q1 Team,
We use TS5A3159A to achieve video signal switch. The frequency is 41MHz and 36MHz. Could you help find the better crosstalk part…
Part Number: TS3A5223 Other Parts Discussed in Thread: TS5A23159 , TS5A23157 , TMUX1136 , TMUX154E Hello team,
Customer is using TS3A5223 on a production project, interfacing a 3MHz clock. There is some unusual behavior being observed on the board and after…
Hi Danny,
We don't have a new device that is p2p compatible with the TS3A24159DGSR.
You can look at the new TMUX1136 in similar configuration and package. You can see more details for new devices in the device search tool here .
You can see by those…