For full duplex to half duplex conversion, you can refer to this diagram.
The TMUX6121 (Hi-RON mux)
Will support +/-16.5V VDD and VSS
The signal on S/D pin will still be rail to rail between VDD and VSS
The digital control pins support 2V logic.
Hi Shai,
The Continuous current for TS12A4514 is ±20mA – depending on the signal direction, the switch supports 20mA.
For a switch to drive 12V, 30mA continuous current, you can use the following below recommended switches:
TS12A12511 :…
Part Number: REF5040 Other Parts Discussed in Thread: TMUX6121 I am using the REF5040 in a new design. The version in the VSSOP 8-pin package has a pin pitch of 0.65mm according to the datasheet.
In the same new design, I am also using the TMUX6121. The…
Shidara,
You can use the ti.com switch selection tool to filter the devices that support these requirements. It looks like these devices will support up to 30mA with TMUX6121. What are you connecting to these devices that you need to support 50mA?
…
Part Number: TMUX6111 Other Parts Discussed in Thread: TMUX6121 In a new design, I need to reduce the off-state leakage as much as possible. The TMUX61xx family looks pretty good. I am actually planning to use the TMUX6121, but that PN was not recognized…
Other Parts Discussed in Thread: TS5A21366 , SN74LVC2G66-Q1 , TMUX6121 Do you have any RS-485 compliant termination selector which is controlled by one of the Digital output of the micro controller
Application would be RS-485 transceiver where the termination…
Carlos,
Do you have the part number of the obsolete device?
I'm not familiar with the CCD camera circuit. What are you connecting to the switch?
You can use the switch selection tool on ti.com to filter for 2-channel devices with dual supplies and…