Part Number: TMUX7462F Tool/software: Hi, Staff
In TMUX7462F(SCDS394B) page30 Figure9-2.
I think the DRAIN voltage changed because the source voltage exceeded the VDD threshold VFP, but why did the DRAIN voltage drop to 0(ZERO)V?
Is it because the…
Part Number: TMUX7236 Other Parts Discussed in Thread: ESDS552 , TMUX7462F Tool/software: Hello all,
I'm currently implementing the TMUX7236 in a design that should be able to switch between AI/RS485. I would like to protect this line from over/under…
Part Number: TMUX7411F Other Parts Discussed in Thread: TMUX7412F , TMUX7413F , TMUX7462F Tool/software: The datasheet lists for the following devices, TMUX7411F / TMUX7412F / TMUX7413F, that TSSOP is listed as preview package.
The last datasheet…
Good morning, Kameron! Do you know if there are SPICE models available somewhere other than the TI Website for this component. I'd like to be able to verify this design with simulation data but I don't think the provided IBIS models will be able to fully…
Part Number: TMUX1574 Other Parts Discussed in Thread: TMUX7309F , TMUX7462F Hello,
I need to implement protection on the TMUX1574 inputs against 60V, I am wondering if this CMOS chip has protection diodes to VCC and GND or not. If there are diodes…
Other Parts Discussed in Thread: TIOL111 , TMUX7412F , TMUX7462F We currently have a design that offers 10-20 discrete IOs that can be programmed as either TTL or avionics voltages (up to 32V). The IOs can be either inputs or outputs. As an option we…
Part Number: TMUX7413F Other Parts Discussed in Thread: TMUX7462F , TMUX7412F , TMUX1574 , TMUX7436F Good afternoon,
I am working on a senior project for WSU's EE program. Currently I am designing a PCB.
As of now, my group is planning to use KiCad…
Other Parts Discussed in Thread: TMUX7462F Hi,
I'm looking for a protection IC for UART communication, to avoid the cirtuit being damaged by the short circuit between power wire (24V or 32V) and RX or TX wire (5V) .
The communication could be stopped…
Part Number: OPA810 Other Parts Discussed in Thread: TMUX7462F , TL072 , TL082 Input signal range: 0 to 10V, single ended signal, frequency 2MHz. The following design is recommended in the user manual. OPA810 input uses 33 Ω+220pf as the filter. Can you…
Other Parts Discussed in Thread: TMUX7462F , TMUX7308F , TMUX7412F , TMUX1072 Hi, TI expert
The customer has an inquiry about overvoltage/reverse polarity voltage protection device.
The required specifications are as follows.
------------------…