Other Parts Discussed in Thread: TPA2026D2 Hi
In the data sheet it is writen that the amp can provide 3.2W from each port.
I am using its EVM and connecting the vdd to power supply that is set on 5V and connect 8ohm 5W speaker..
Using the EVM software…
Other Parts Discussed in Thread: TPA2016D2 , TPA2026D2 , TPA0213
I want to connect the TPA2026D2 (not TPA2016D2) output as above because the pin number of the accessory interface is not enough. Can I do so? What problems will this? Thanks very much!
Dear Don.
In case of Single Ended usage, what is the guaranteed maximum speaker output power from TPA2026D2 at a given 5V and 4 Ohm speaker load? Can I assume the output power is almost half of differential input ?
Thanks & BR
Other Parts Discussed in Thread: TPA2026D2 Hi,
Iam Using TPA2026D2 Stereo amplifier,Iam Driving Speaker thru below
DSPIC(Micro controller PWM Pins)==>RC Low pass filter==>Stereo Amplifier==>Speaker.
I used RC low pass filter, i would like to…
Other Parts Discussed in Thread: TPA2026D2 Hi,
Just gotten an eval kit for TPA2026D2. Was looking thru the user guide and it states that it can be evaluated in stand-along mode or connected to ccts with I2C controls.
Standalone mode should be clear cut…
Other Parts Discussed in Thread: TPA2026D2 what is the input impedance of TPA2026d2? Can I chain the input of TPA2026 together with another amplifier input (also differential), with DC blocking cap to separate them of course. I think I can but the TPA2026…
Hi Sakamoto-san,
Welcome to e2e.
You may be interested in moving from TPA2016D2 to TPA2026D2. Most likely the volume ramp you describe is native from TPA2016D2, and this was changed for TPA2026D2 as described in Figure 27 from data sheet .
Best regards…
Hi, Zoe,
The TPA2026D2 or TPA2008D2 could be some options, in case you are interested in a device with a power supply range up to 5.5V.
In case of higher power supply range, the TPA3132D2 could be also a replacement.
Best regards, Luis Fernando Rodríguez…
Sara,
If digital input is an option, you can consider TAS2557 or TAS2563. These are SmartAmps that feature embedded processing for speaker protection algorithms, which avoid harmful events for the speaker like clipping, over-excursion and over-heating…