Part Number: TPA2028D1 Other Parts Discussed in Thread: TLV320AIC3101
Hello,
I am encountering an issue with high transient currents when using the TPA2028D1 to drive a 2.5W speaker, and I would appreciate some analysis.
System Setup…
Part Number: TPA2028D1 I am looking at TPA2028, the class D DRC IC.
The project I am working on is: input is voice signal amplitude range from 0.3VPP to 5.5V VPP with DC offset 0V, frequency range from 80Hz to 3KHz. Output needs to be voice signal amplitude…
Part Number: TPA2028D1 Hello. It's not stated in the datasheet if the EN pin can be left floating for an "always enabled" application. I don't have a dev kit to test. I would appreciate an answer as this is the only BGA component on our board, and the…
Part Number: TPA2028D1 Other Parts Discussed in Thread: TLV320AIC3101 Tool/software: Hi ,
My product uses codec TLV320AIC3101 and OA TPA2028D1YZF to drive 4-ohm speakers with power ranging from 2.5W to 3W. I have completed the schematic design. I noticed…
Part Number: TPA2028D1
Tool/software:
We utilize the TPA2028D1 as the SPK AMP, and the normal settings are as follows:
``` i2cset -y -f 2 0x58 0x01 0xC3 w i2cset -y -f 2 0x58 0x02 0x3F w i2cset -y -f 2 0x58 0x03 0x02 w i2cset -y -f 2 0x58 0x04 0x18…
Part Number: TPA2028D1 Tool/software: Hello support community!
We are trying to understand the state of OUT+ and OUT- when EN is set to 0. The datasheet mentions that OUT+ and OUT- will have 2 kohm impedance. Is this impedance with respect to GND or…
Part Number: TPA2028D1 Other Parts Discussed in Thread: TPA2016D2 Hi team,
Do you have similar function as the TPA2028D1 but with EVM and meet below requirement?
Main requirement is DRC configured to protect the Steps (when compression is used) speaker…
Part Number: TPA2028D1 Tool/software: Hello,
I’m working on a project using the Smart AMP TPA2028D1 , and I have a speaker with 4Ω impedance .
I would like to set the Limiter Power Level to 2.3W , since that is the desired maximum power output for…
Part Number: TPA2028D1 Hello I am Luis
Let me ask a question.
I have a question TPA2028D1 volume control
[test circuit]
input 1kHz sinewave to IN+, IN- and attach RC filter(R-1kohm, -4.7nF) to OUT+, OUT -
and input signal 1kHz sinewave and…
Part Number: TPA2028D1 Hi
Can I use TPA2028 for both products?
One set of speakers is connected to 2W/4Ω (set Max.<2.5W)
The other group is connected to the speaker 1W/7Ω (set Max.<0.02W)