Hi Rory,
You could have a look at next device: TPA2029D1. This device has an AGC and doesn't have an I2C circuit.
You can use the TPA2028D1 without I2C, but the device will work with the default setting.
Best Regards
José Luis Figueroa
Audio Applications…
Hi Ajit,
The maximum input voltage is Vdd+0.3V according to the Absolute Maximum Ratings section in the device's datasheet. You can have a look at the following devices: TPA2015D1, TPA2028D1, and TPA2029D1. All of them are Class-D Audio Amplifiers…
Part Number: TPA6132A2 Other Parts Discussed in Thread: TPA2029D1 I have system that extract audio data from a car power amplifier and feeds it to a computer mic input. My main problem is the gain control, the output of the amplifier is too high for the…
Other Parts Discussed in Thread: LM4930 , TPA2029D1 Hi sir:
If LM4930 use external class D amplier,how to connect?Can I connet LM4930's pin(E2) LS- and pin(F2) LS+ to external PA‘s input pin?
thanks!
Other Parts Discussed in Thread: TINA-TI Update of TINA9-TI Spice Model Libraries and Example Circuits
This note describes the step-by-step process for updating the TINA9-TI Spice Macro Libraries and Example circuits. The update is initiated by selecting…